LPC54018 IoT board & Amazon Freertos: UsageFault coprocessor

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC54018 IoT board & Amazon Freertos: UsageFault coprocessor

1,483 Views
ybdecawave
Contributor I

Hello,

I am using the LPC54018 IoT board with the baseboard, and when I try to run the aws echo example on it, I have a UsageFault coprocessor after the scheduler starts. #

I'm using Segger embedded studio. I've tried to erase the MCU severall time to start from scratch, but I really can't get rid of this error. It is a bit surprising since I'm using software directly downloaded from segger website.

https://www.segger.com/downloads/eval/amazon-freertos-lpc54018.zip 

I wanted to try with MCUXpresso, but I cannot see the aws examples in the LPC018-IoT board SDK 2.3. Do you have a direct link to this SDK ? (I've downloaded it with the MCUXpresso SDK builder but there is no aws examples as far as I can see )

Thanks for the help,

Best regards

Yves

Labels (4)
0 Kudos
Reply
1 Reply

1,152 Views
soledad
NXP Employee
NXP Employee

Hi,

1. Please go the following link:

Welcome | MCUXpresso SDK Builder 

2. Click on select development board

pastedImage_3.png

3. You need to sign  in.

pastedImage_4.png

4. Select the board and name.

pastedImage_5.png

5. Click on the Build MCUXpresso SDK

pastedImage_7.png

6. Select the IDE

pastedImage_6.png

7. Click on Add Software component

pastedImage_8.png

8. Select the software component needed  and click on save changes.

pastedImage_10.png

9. Click on Download SDK.

pastedImage_11.png

10. After download the SDK you will find the aws_examples

pastedImage_12.png

I hope this helps,

Have a great day,
Sol
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply