LPC4370 / Is it possible to apply a specified voltage to the USB pin when the device power is off?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC4370 / Is it possible to apply a specified voltage to the USB pin when the device power is off?

Jump to solution
1,178 Views
yasushihasegawa
Contributor III

Dear All,

Our device is implemented with LPC 4370.
There is a question about the case where our device is not powered on and voltage is supplied from the target host side via the USB cable.

[Background]
(1) Our device is a USB device, not a host.
(2) Our device is "self-powered device", not "bus-powered device".
(3) The other USB host device and our device are connected by a USB cable, and a voltage within the specified range is supplied to the USB cable from the USB Host device.

[conditions]
(1) The device power supply is OFF, and the following pins of LPC4370 are not powered.

  VDD (IO)
  VDD (REG) (3 V 3)
  VDDA (3 V 3)
  USB0_VDDA3V_DRIVER
  USB 0 _ VDDA 3 V 3
  Vprog (pf)

(2)Voltage is applied to our device from the other host's side via the USB cable under the above conditions.

[Question]
Is there a problem in applying a voltage within the specified range to the following USB pins of LPC 4370? 
In other words, will internal latch-up and malfunctions not occur?

  Pin name / specified range
  USB0_VBUS / min 0[V], max 3.6[V]
  USB0_DP / min 0[V], max 3.6[V]
  USB0_DM / min 0[V], max 3.6[V]
  USB0_ID / min 0[V], max 3.6[V]

Best Regards,
Yasushi

0 Kudos
Reply
1 Solution
997 Views
soledad
NXP Employee
NXP Employee

Hi,

The data sheet provides absolute max rates for a scenario similar to yours (Vddio=0v) as it is specified in table 10. pastedImage_1.png

so you shouldn't have issues if you are careful with voltage spikes when restoring the supply to the device.

Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

2 Replies
998 Views
soledad
NXP Employee
NXP Employee

Hi,

The data sheet provides absolute max rates for a scenario similar to yours (Vddio=0v) as it is specified in table 10. pastedImage_1.png

so you shouldn't have issues if you are careful with voltage spikes when restoring the supply to the device.

Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

997 Views
yasushihasegawa
Contributor III

Dear Soledad,

Thank you for your support.
I satisfy with your answer and advice.

Best Regards,
Yasushi Hasegawa

0 Kudos
Reply