I am programming using an LPC4370 to acquire data at 80msps, I am transferring data using USB communication. Although I think I have set all the required ADCHS configurations, I still only get it to run at 40msps if I do FFT of the data after acquisition. Please let me know what I might have to do.
I have attached a part of my codes, and I am using the libraries of NXPOpen.
void initialize_hsadc(void) { LPC_ADCHS->POWER_DOWN = 0; LPC_ADCHS->FLUSH = 1; Chip_HSADC_Init(LPC_ADCHS); LPC_ADCHS->FIFO_CFG = (15 << 1) /* FIFO_LEVEL*/ | (1); /* PACKED_READ*/ LPC_ADCHS->DSCR_STS = 1; //NOTE: CH0 LPC_ADCHS->DESCRIPTOR[0][0] = (1 << 31) /* UPDATE TABLE*/ | (1 << 24) /* RESET_TIMER*/ | (0 << 22) /* THRESH*/ | (0xA00 << 8) /* MATCH*/ | (0x10 << 6); /* BRANCH*/ //NOTE: CH1 LPC_ADCHS->DESCRIPTOR[1][0] = (1 << 31) /* UPDATE TABLE*/ | (1 << 24) /* RESET_TIMER*/ | (0 << 22) /* THRESH*/ | (0x01 << 8) /* MATCH*/ | (0x01 << 6); /* BRANCH*/ LPC_ADCHS->CONFIG= (0x90 << 6) /* RECOVERY_TIME*/ | (0 << 5) /* CHANNEL_ID_EN*/ | (0x01) /* TRIGGER_MASK*/; const uint8_t kDGEC = 0xE; LPC_ADCHS->ADC_SPEED = (kDGEC << 16) | (kDGEC << 12) | (kDGEC << 8) | (kDGEC << 4) | (kDGEC); //Didn't set threshold registers as they aren't used LPC_ADCHS->POWER_CONTROL = (1 << 18) /* BGAP*/ | (1 << 17) /* POWER*/ | (1 << 10) /* DC in ADC0*/ | (1 << 4) | (0x4); /* CRS*/ } void setup_dma(void){ //DMA settings Chip_GPDMA_Init(LPC_GPDMA); // Initialize the GPDMA LPC_GPDMA->CONFIG = 0x01; while( !(LPC_GPDMA->CONFIG & 0x01) ); /* Clear all DMA interrupt and error flag */ LPC_GPDMA->INTTCCLEAR = 0xFF; //clears channel terminal count interrupt LPC_GPDMA->INTERRCLR = 0xFF; //clears channel error interrupt. LPC_GPDMA->CH[DMA_CH].SRCADDR = (uint32_t) &LPC_ADCHS->FIFO_OUTPUT[0]; LPC_GPDMA->CH[DMA_CH].DESTADDR = ((uint32_t) &sample); LPC_GPDMA->CH[DMA_CH].CONTROL = (TRANSFER_SIZE_DMA) // transfer size | (0x0 << 12) // src burst size | (0x0 << 15) // dst burst size | (0x2 << 18) // src transfer width | (0x2 << 21) // dst transfer width | (0x1 << 24) // src AHB master select | (0x0 << 25) // dst AHB master select | (0x0 << 26) // src increment: 0, src address not increment after each trans | (0x1 << 27) // dst increment: 1, dst address increment after each trans | (0x1 << 31); // terminal count interrupt enable bit: 1, enabled LPC_GPDMA->CH[DMA_CH].CONFIG = (0x1 << 0) // enable bit: 1 enable, 0 disable | (HSADC_DMA_READ << 1) // src peripheral: set to 8 - HSADC | (0x0 << 6) // dst peripheral: no setting - memory | (0x6 << 11) // flow control: peripheral to memory - DMA control | (0x1 << 14) // IE - interrupt error mask | (0x1 << 15) // ITC - terminal count interrupt mask | (0x0 << 16) // lock: when set, this bit enables locked transfer | (0x1 << 18); // Halt: 1, enable DMA requests; 0, ignore further src DMA req LPC_GPDMA->CH[DMA_CH].LLI = 0; }
/* Bit Manipulation for USB communication */ for(int i = 0; i < a1; i++){ sample_tx[2*i+1] = (uint8_t)(sample[i]>>8); sample_tx[2*i] = (uint8_t)sample[i];
} /* Sending the USB Data */ while (libusbdev_Connected()) { libusbdev_Send(&sample_tx[0], sizeof(sample_tx)/sizeof(sample_tx[0])); break; // Break out of the loop once the data is sent }
Thanks in advance!
Hi, Visweshwar,
How do you know that the ADC sampling frequency is 40MSPS instead of 80MSPS?
BR
XiangJun Rong