LPC4357JBD208E vs LPC4357JBD208K

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC4357JBD208E vs LPC4357JBD208K

Jump to solution
1,118 Views
amirnat
Contributor I

Hi, what is the difference between LPC4357JBD208E and LPC4357JBD208K ?

I searched in some distributors like Mouser and Digikey, they suggest to buy LPC4357JBD208K instead of LPC4357JBD208E, why? Is there any failure  or other issue? 

I have created a C project for LPC4357JBD208E, can I run it on LPC4357JBD208K

Are LPC4357JBD208E and LPC4357JBD208K pin compatible? can I solder LPC4357JBD208K instead of LPC4357JBD208E?

thank you in advance.

 

0 Kudos
1 Solution
1,097 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Amir,

The answer is Yes, the silicon are the same for the LPC4357JBD208E and LPC4357JBD208K, you can  replace any of them with each other without any software and/or hardware consideration.

BR

XiangJun Rong

View solution in original post

0 Kudos
4 Replies
1,108 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

Pls refer to the link:

https://www.nxp.com/products/processors-and-microcontrollers/arm-microcontrollers/general-purpose-mc...

 

The LPC4357JBD208E package contains 36 PCS, but the LPC4357JBD208K package contains 180 PCS.

LPC4357JBD208E

Active

 

LPC4357JBD208K

Active

Hope it can help you

BR

XiangJun Rong

0 Kudos
1,103 Views
amirnat
Contributor I

Thank you dear  xiangjun_rong,

Can I replace any of them with each other without any software and/or hardware considerations?

0 Kudos
1,098 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Amir,

The answer is Yes, the silicon are the same for the LPC4357JBD208E and LPC4357JBD208K, you can  replace any of them with each other without any software and/or hardware consideration.

BR

XiangJun Rong

0 Kudos
1,094 Views
amirnat
Contributor I

Thank you very much.

0 Kudos