LPC4357: modification of images for DFUsec

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC4357: modification of images for DFUsec

1,435件の閲覧回数
quex
Contributor I

I'd like to download images to my LPC4357 using  DFUSec (Two projects: M4 & M0App).

From the forum I understood, that I need a tool to modify the binaries.

Unfortunately the link does not work any more:

http://lpcware.com/content/nxpfile/lpc18xx-43xx-image-manager

Where could I get the image manager from?

Thanks

ラベル(3)
0 件の賞賛
返信
3 返答(返信)

1,200件の閲覧回数
quex
Contributor I

Thank you, I'll try that.

0 件の賞賛
返信

1,200件の閲覧回数
lpcxpresso_supp
NXP Employee
NXP Employee

DFUSec was superseded by LPCScrypt sometime ago  : http://www.nxp.com/lpcscrypt

Installing LPCScrypt will also provide the "image manager tool", though you don't need this for programming images into internal flash.

Regards,

LPCXpresso Support

0 件の賞賛
返信

1,200件の閲覧回数
soledad
NXP Employee
NXP Employee

Hi,

Please check the below link and let me know if this helps.

USB DFU Firmware Upload for LPC1850 LPC4350 LPC1800 LPC4300 LPC18xx LPC43xx 


Have a great day,
Soledad

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信