LPC4357 + SDRAM (MT48LC8M32B2B5-6 ) interface

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC4357 + SDRAM (MT48LC8M32B2B5-6 ) interface

1,249 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Prabhakaran_Raja on Mon Feb 08 21:14:55 MST 2016
Hi,

I have LPC435x-Xplorer++ board.
I need to interface LPC4357 with SDRAM(MT48LC8M32B2B5-6) over EMC.
i'm using LPCXpresso v7.9.2 IDE.
so can any one suggest me Is there any example or library available for SRAM interface. (over EMC)  
标签 (1)
标记 (1)
0 项奖励
回复
2 回复数

1,050 次查看
soledad
NXP Employee
NXP Employee

Hello,

Please check the below application note, this appnote describes how to properly interface SDRAM memory to the LPC1800 and LPC4300 External Memory Controller.

AN11508: SDRAM interface to LPC18xx/43xx EMC | www.LPCware.com

I hope this helps


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,050 次查看
moller
Contributor II

Did you find a solution? I would be very interested in any help and info I can get my hands on to interface to my 64MB SDRAM.

0 项奖励
回复