LPC4353JBD208 question

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

LPC4353JBD208 question

跳至解决方案
1,535 次查看
uzunov16
Contributor I

Hello, I'm new in fixing electronics. I'm trying to fix my ploter PCB and i cheked with multimeter the capacitors. Every capacitor around the LPC4353JBD208 seems to be shorted. Does that means the MCU is shorted and i need to replace it?

Thank you!

0 项奖励
回复
1 解答
1,495 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

Okay, I suppose the MCU has broken down, you need a new one.

BR

XiangJun Rong

在原帖中查看解决方案

0 项奖励
回复
6 回复数
1,509 次查看
uzunov16
Contributor I

I removed the MCU and now the capacitors are not shorted. That means i need new MCU?

0 项奖励
回复
1,436 次查看
uzunov16
Contributor I

Do i need a software to program the MCU after the replacement?

0 项奖励
回复
1,413 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

The LPC4353 has on-chip flash, I suppose that you have to program your application code to the flash.

If you have the source code project, you can use keil, IAR or MCUXPresso tools to download the code.

If you has the *.bin or S_record file, you can use FlashMagic tools to download the code in ISP mode.

https://www.flashmagictool.com/download.html&d=flashmagic

 

Hope it can help you

BR

XiangJun Rong

0 项奖励
回复
1,496 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

Okay, I suppose the MCU has broken down, you need a new one.

BR

XiangJun Rong

0 项奖励
回复
1,518 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

I suppose that the VDD and GND pins are shorted either on board or inside silicon. Pls remove the LPC4353 from board and check if the shorting happens or not.

Hope it can help you

BR

XiangJun Rong

0 项奖励
回复
1,516 次查看
uzunov16
Contributor I

Thank you! I'll try it.

0 项奖励
回复