LPC4350 SSEL

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC4350 SSEL

1,317 次查看
dudisasson
Contributor I

Hi,

I am using an LPC4350 as an SPI slave, is there a way to disable the use of the SSEL pin or drive it to throw another GPIO?

标签 (1)
0 项奖励
回复
2 回复数

1,141 次查看
soledad
NXP Employee
NXP Employee

Hi,

Please check the below thread and let me know if this helps,

https://community.nxp.com/thread/433611 


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,141 次查看
dudisasson
Contributor I

Hi,

Thank you for the fast reply.

In the thread you suggested, the LPC is the master so the SSEL is an output

to the slave but In my case the LPC is the slave.

Dudi.

בתאריך 4 בינו׳ 2018 18:15,‏ "soledad" <admin@community.nxp.com> כתב:

NXP Community

<https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg>

Re: LPC4350 SSEL

reply from soledad

<https://community.nxp.com/people/soledad?et=watches.email.thread> in

LPC - View the full discussion

<https://community.nxp.com/message/974577?commentID=974577&et=watches.email.thread#comment-974577>

0 项奖励
回复