thank you!
Hi peng dacheng,
Although the datasheet you can check the difference between the MCU, in this case, the LPC4333 an LPC4330 are pin to pin compatible, with the only difference that the LPC4333 has an internal flash, so in case that you use that MCU you do not need an external.
Also, you can find the LPC4333 with the TFBGA100 package, in the link below LPC4333JET100.
Wish it helps you!
regard,
Miguel
翻译:
你好 peng dacheng,
虽然数据表可以检查MCU之间的差异,但在这种情况下,LPC4333和LPC4330是引脚兼容的,唯一不同的是LPC4333有一个内部闪存,因此如果您使用该MCU,则不需要外在的。
此外,您还可以在LPC4333JET100下方的链接中找到带有TFBGA100封装的LPC4333。
希望它能帮到你!
看待,
Miguel