LPC4088 and external SDRAM issues

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC4088 and external SDRAM issues

2,751 次查看
mark82
Contributor III

Good morning. I've been working on a custom board based on LPC4088 and external SDRAM chip IS42S16400J, under IAR EWARM 6.70. 

The CPU is set to run at 108Mhz and the EMC a 54Mhz.

I'm using the init routines from the LPCOPEN bundle v2.10 (I think it's the latest one). 

The chip is mapped to block 0 (address 0xA0000000).

I customized the init structure for my memory chip as follows: 

STATIC const IP_EMC_DYN_CONFIG_T IS42S16400J_6BL_config = {
     EMC_NANOSECOND(64000000 / 4096),
     0x01,                    /* Command Delayed */
     EMC_NANOSECOND(15),     /* tRP */
     EMC_NANOSECOND(42),     /* tRAS */
     EMC_NANOSECOND(66),     /* tSREX */
     EMC_NANOSECOND(15), /* tAPR */     //Using trp
     EMC_CLOCK(3),          /* tDAL */
     EMC_CLOCK(2),          /* tWR */
     EMC_NANOSECOND(60),     /* tRC */
     EMC_NANOSECOND(66),     /* tRFC */
     EMC_NANOSECOND(66),     /* tXSR */
     EMC_NANOSECOND(12),     /* tRRD */
     EMC_CLOCK(0x02),     /* tMRD */
     {
          {
               EMC_ADDRESS_DYCS0,     /* EA Board uses DYCS0 for SDRAM */
               2,     /* RAS */

               EMC_DYN_MODE_WBMODE_PROGRAMMED |
               EMC_DYN_MODE_OPMODE_STANDARD |
               EMC_DYN_MODE_CAS_2 |
               EMC_DYN_MODE_BURST_TYPE_SEQUENTIAL |
               EMC_DYN_MODE_BURST_LEN_8,

               EMC_DYN_CONFIG_DATA_BUS_16 |
               /*EMC_DYN_CONFIG_LPSDRAM |*/
               EMC_DYN_CONFIG_4Mx16_4BANKS_12ROWS_8COLS |
               EMC_DYN_CONFIG_MD_SDRAM
          },
          {0, 0, 0, 0},
          {0, 0, 0, 0},
          {0, 0, 0, 0}
     }
};

I just added a missing RBC check that I got from LPC43XX sourc code. It's the following:

/* is it high performance RBC mode? */
          if (!(Dynamic_Config->DevConfig[ChipSelect].DynConfig & EMC_DYN_CONFIG_LPSDRAM)) {
               /* yes, it is */
               /* getting the number of banks  */
               if (!(Dynamic_Config->DevConfig[ChipSelect].DynConfig & (0x7 << EMC_DYN_CONFIG_DEV_SIZE_BIT))) {
                    /* 2 banks => 1 bank select bit */
                    Col_len += 1;
               }
               else {
                    /* 4 banks => 2 bank select bits */
                    Col_len += 2;
               }
          }

Well, I think I said everything, but just ask if you need more details. So I can describe "the symptoms". 

After initialization of EMC controller and SDRAM chip, my app executes some SDRAM tests that are ALWAYS passed with success. These tests are taken from the LPCOPEN projects mentioned above (mem_tests.c, which contains the walking tests and pattern tests). It also passes succesfully some other tests we had already used in the past. 

I'm still in debugging phase of the project, so my code continuously runs some debug checks such as writing some placehoders bytes in my structured variable placed in the external RAM and reads them back. After less than a minute one of this byte is written badly: 0xAF instead of  0xAA. It's deterministic. On the other hand this symptom is raised immediately as soon as I put this structured variable in the "Live Watch" window in IAR. Surely the debugger triggers accesses to the external RAM to show me that variable. This structured variable is about 17Kbytes.

Also, while debugging, I get bad writings at the same positions and with the same bad values. 

My attempts to solve the problems were:

- Lower the frequencies of CPU to 60Mhz and EMC to 30Mhz;

- "Playing" a little with the timings of the chip;

- Trying different settings such as RBC and BRC, busrt types...;

In most cases I had no changes and sometimes the tests failed.

Thanks for your time.

Marco

标签 (2)
标记 (4)
0 项奖励
回复
4 回复数

2,116 次查看
jeremyzhou
NXP Employee
NXP Employee
Thank you for your interest in NXP Semiconductor products and 
the opportunity to serve you.
To provide the fastest possible support I want to point you to a 
similar question which has been answered on our NXP community. 
Please refer to External SDRAM with EMC 
to view the details.
Have a great day,

TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

2,116 次查看
mark82
Contributor III

Thanks for your reply, @jeremyzhou.

I had already read the discussion you linked, such other one in the community, but I could find anything that could solve my problem.

I also tried again the configuration of timing from your last reply, but they make the tests fail. 

Also tried to modify the fine tuning of the clock delay in EMCDLYCTL register. 

Also checked again GPIOs to be set to correct functions. Here's the code that inits pins:

#define SDRAM_PIN_IOCON_VALUE     0x201     //Fast slew rate and function 0x01
void BSP_SDRAM_Init(void)
{
     // Assign pins to SDRAM controller
     
     //CAS
     IOCON_P2_16 = SDRAM_PIN_IOCON_VALUE;
     
     //RAS
     IOCON_P2_17 = SDRAM_PIN_IOCON_VALUE;
     
     //SDCLK
     IOCON_P2_18 = SDRAM_PIN_IOCON_VALUE;
     
     //SDCS
     IOCON_P2_20 = SDRAM_PIN_IOCON_VALUE;
     
     //SDCLKEN
     IOCON_P2_24 = SDRAM_PIN_IOCON_VALUE;
     
     //DQMN0..1
     IOCON_P2_28 = SDRAM_PIN_IOCON_VALUE;
     IOCON_P2_29 = SDRAM_PIN_IOCON_VALUE;
     
     //DATA BUS
     IOCON_P3_00 = SDRAM_PIN_IOCON_VALUE;
     IOCON_P3_01 = SDRAM_PIN_IOCON_VALUE;
     IOCON_P3_02 = SDRAM_PIN_IOCON_VALUE;
     IOCON_P3_03 = SDRAM_PIN_IOCON_VALUE;
     IOCON_P3_04 = SDRAM_PIN_IOCON_VALUE;
     IOCON_P3_05 = SDRAM_PIN_IOCON_VALUE;
     IOCON_P3_06 = SDRAM_PIN_IOCON_VALUE;
     IOCON_P3_07 = SDRAM_PIN_IOCON_VALUE;
     IOCON_P3_08 = SDRAM_PIN_IOCON_VALUE;
     IOCON_P3_09 = SDRAM_PIN_IOCON_VALUE;
     IOCON_P3_10 = SDRAM_PIN_IOCON_VALUE;
     IOCON_P3_11 = SDRAM_PIN_IOCON_VALUE;
     IOCON_P3_12 = SDRAM_PIN_IOCON_VALUE;
     IOCON_P3_13 = SDRAM_PIN_IOCON_VALUE;
     IOCON_P3_14 = SDRAM_PIN_IOCON_VALUE;
     IOCON_P3_15 = SDRAM_PIN_IOCON_VALUE;
     
     //ADDRESS BUS
     IOCON_P4_00 = SDRAM_PIN_IOCON_VALUE;
     IOCON_P4_01 = SDRAM_PIN_IOCON_VALUE;
     IOCON_P4_02 = SDRAM_PIN_IOCON_VALUE;
     IOCON_P4_03 = SDRAM_PIN_IOCON_VALUE;
     IOCON_P4_04 = SDRAM_PIN_IOCON_VALUE;
     IOCON_P4_05 = SDRAM_PIN_IOCON_VALUE;
     IOCON_P4_06 = SDRAM_PIN_IOCON_VALUE;
     IOCON_P4_07 = SDRAM_PIN_IOCON_VALUE;
     IOCON_P4_08 = SDRAM_PIN_IOCON_VALUE;
     IOCON_P4_09 = SDRAM_PIN_IOCON_VALUE;
     IOCON_P4_10 = SDRAM_PIN_IOCON_VALUE;
     IOCON_P4_11 = SDRAM_PIN_IOCON_VALUE;
     IOCON_P4_12 = SDRAM_PIN_IOCON_VALUE;
     IOCON_P4_13 = SDRAM_PIN_IOCON_VALUE;
     IOCON_P4_14 = SDRAM_PIN_IOCON_VALUE;
     
     //SDWE
     IOCON_P4_25 = SDRAM_PIN_IOCON_VALUE;
     
     /*Init SDRAM controller*/
     
     /* Setup EMC Delays */
     /* Move all clock delays together */
     LPC_SYSCTL->EMCDLYCTL = (CLK0_DELAY) | (CLK0_DELAY << 8) | (CLK0_DELAY << 16 | (CLK0_DELAY << 24));
     
     /* Init EMC Controller -Enable-LE mode- clock ratio 1:1 */
     Chip_EMC_Init(1, 0, 0);
     
     /* Init EMC Dynamic Controller */
     Chip_EMC_Dynamic_Init((IP_EMC_DYN_CONFIG_T *) &IS42S16400J_6BL_config);
}

I'm attaching schematic images, too.

LPC4088 and RAM-page-001.jpgLPC4088 and RAM-page-002.jpg

Still encoutering thos issues.

Thanks,

Marco

0 项奖励
回复

2,116 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi Marco Fratini

After confirming, the LPC4088 OEM BOARD integrates the SDRAM IS42S32800D whose electrical characteristics are compatible with the IS42S16400J, so I'd highly recommend you to refer to the memtest demo in the lpcopen_2_10_lpcxpresso_ea_devkit_4088.

LPCOpen Software for LPC40XX|NXP 

2017-09-15_15-37-52.jpg


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

2,116 次查看
mark82
Contributor III

Thanks for you reply, jeremyzhou.

The demo project you mentioned was the one I startet from. I changed the IS42S32800D parameters accordingly to my memory chip (like some timings, row bank columns, bus width and so on). My code also performs the mem_tests from the demo (walking0, walking1, etc..). So, I had already tried those values.

The only differences I see from schematics are the series resistors in data lines and the fact that I scrambled the data lines to avoid vias in PCB layout.

But, before thinking about 22R series resistors as possible cause, I'm trying to solve the problem by adjusting software.

As last, the data line scrambling should be safe (we have another board with LPC1788, with data lines scrambled and no resistors, that works fine). 

The failure in sdram occurs after a while in free running, or as soon as I observe the sdram from "Live Watch". Rarely it doesn't occur at all. 

Thanks,

Marco

0 项奖励
回复