LPC4078 pins p0[29] and p0[30] not boundary scan senseable

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC4078 pins p0[29] and p0[30] not boundary scan senseable

1,465 Views
MD1
Contributor I

Hello,

in the .bsdl file of the mentionen controller, both pins are defined as "linkage" and not as "inout". Is this intended?

I can not read out these pins in my BS tool.

 

Thanks and best regards

Labels (1)
0 Kudos
Reply
3 Replies

1,456 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @MD1 

What about the complete part number name? 

Only the two pins can not read out, other pins can work well?

 

BR

Alice

0 Kudos
Reply

1,444 Views
MD1
Contributor I

Hello @Alice_Yang,

the complete part number would be LPC4078FBD100 with its BSDL file.

Yes, other pins work as expected, just those two do not.

 

Best regards

0 Kudos
Reply

1,420 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @MD1 ,

I have confirmed with our SE, the pin marked as "linkage" means can not read out.

 

BR

Alice

0 Kudos
Reply