LPC2478 LCD clock

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC2478 LCD clock

1,950 次查看
sivaramakrishna
Contributor I

HI,

I have configured the LPC2478 LCDDCLK clock to 24MHz O/P and observed that the clock is not reaching to full 0VDC on the negative transition.

I have made the following measurements and observe the issue:

1) Configured the DCLK at Pin 150 to 14MHz and observed the sine wave clk  with slow rise and fall times.

2) When it is configured to 24MHz clock the clock signal is not  reaching to complete 0VDC on the negative transition.

Can you please suggest the root cause and possible trouble shooting techniques on this.Measurement WF are attached for reference.

Thanks ,

Siva Bommaraju

标签 (1)
标记 (1)
0 项奖励
回复
1 回复

1,784 次查看
CarlosCasillas
NXP Employee
NXP Employee

Hi Siva,

If you are using a custom board, you should verify the general design recommendations for clock signals, as it seems to be hardware related (i.e. unbalanced impedances/capacitances).

As complementary information, you could take a look to the following links:

https://www.nxp.com/docs/en/application-note/AN10778.pdf

http://www.onarm.com/forum/20290/


Hope this will be useful for you.
Best regards!
/Carlos
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复