Hi,
I am working on a project, which has a one module of TCPIP communication. But before I had used a PIC32 microchip controller which is shipped with a in-build mac address, what in case of LPC2388 and LPC1788, does it have a in-build mac address or I need to assign, how I can assign the unique mac address.
thanks & regards
Mohammad Faizan
Hello Mohammed
The MAC-address can be entered via the 'Station Addresses'.
See User Manual UM10211. Search on 'Station Address'.
See: http://www.lpcware.com/content/nxpfile/lpc23xx-user-manual
But (...) NXP does not supply MAC addresses for its products. The only way, I see, is to buy them from the IEEE:
http://standards.ieee.org/regauth/oui/index.shtml
https://standards.ieee.org/regauth-bin/application?rt=OUI
You buy a block of 16 million addresses, and that currently costs you (?) $1825.
There is an Application Note handeling about connecting the LPC2000 with ethernet, see:
http://www.lpcware.com/content/nxpfile/an10403-connecting-ethernet-interface-lpc2000