Hi
It is running production design changes, thus
Option1 :
We would like to keep Micro family similar if we can not find pin-pin replacement, micro frequency similar
1. Family : ARM7 same as LPC2292FBD144/01.5
2.Core Size : 32bit same as LPC2292FBD144/01.5
3. Speed : 60MHz same as LPC2292FBD144/01.5
4. Connectivity : > = 1 CANbus, EBI/EMI, >=1 I²C, Microwire, >=1 SPI, SSI, SSP, >=1 UART/USAR
5. Peripherals : POR, PWM, WDT
6. No of IO >= 112
7. Program memory >= twice the current memory 256KB (256K x FLASH
8. RAM size >= twice the current size 16K x 8
9. A/D >= 8x10b i.e 12-bit preferred.
Option2 : New micro family with above minimum requirement which will require significant amount of work and as it is running production change we may not proceed with option2.