Dear Support,
Thanks for that info.
I am using USB1 so i have the jumper links set to:
P1_1 = L
P1_2 = H
P2_8 = H
P2_9 = L
This is what is detailed in section 3.1. I am not using OTP and the ISP link is open.
I though it might be my code, so i tried an example code in the images folder of the LPCScrypt folder -> MCB1800_blinky_BankA.bin.
I blanked the memory using the JTAG and then programmed the device using the MCB1800_blinky_BankA program and it downloaded OK. but again i can not download any more. I have tried a number of tests, power cycling the device etc and still have comms.
I followed section 3.1.
Is there a software parameter which also controls the Boot mode?
Any help would be appreciated.
Thanks
Andrew