LPC1857 TCP/IP packet loss

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC1857 TCP/IP packet loss

Jump to solution
2,221 Views
rubensjunior
Contributor IV

Hi friends! I am facing a problem with TCP/IP packet loss. My circuit uses the LPC1857 microcontroller and as an interface for the ethernet connection I use the LAN8720 IC. What could be causing the loss of many packets in the ping test for example?

Thanks a lot!

Rubens Júnior

 

Labels (3)
0 Kudos
Reply
1 Solution
2,183 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

This is my guess, maybe the core is overloaded, pls remove or disable the other interrupt, enable only the ethernet interrupt and have a try.

BR

XiangJun Rong

 

View solution in original post

2 Replies
2,162 Views
rubensjunior
Contributor IV

Hi @xiangjun_rong ! Thanks a lot!

0 Kudos
Reply
2,184 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

This is my guess, maybe the core is overloaded, pls remove or disable the other interrupt, enable only the ethernet interrupt and have a try.

BR

XiangJun Rong