LPC1837 with SPIFI

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC1837 with SPIFI

3,287 次查看
jan92
Contributor II

Hello,

I would like to use the spifi memory as a storage for my data. I tried the example "lpcspifilib" which seems to work fine. Problem is when I only want to read the written data after the reset of the program. It reads only 0xFF like if the memory was erased. Any ideas what could be the problem?

Thanks for help.

Jan

标签 (1)
标记 (2)
0 项奖励
回复
3 回复数

3,026 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi Jan Hakl,

Thank you for your interest in NXP Semiconductor products and 
the opportunity to serve you.
I was wondering if you can tell me what SPIFI device you use and share the sample code you run.
Have a great day,

TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

3,026 次查看
jan92
Contributor II

Hi Jeremy,

It is the sample code: lpcspifilib

First i run this code, which seems fine:

static void RunExample(void)
{
uint32_t idx;
uint32_t spifiBaseClockRate;
uint32_t maxSpifiClock;
uint16_t libVersion;
uint32_t pageAddress;
uint32_t loopBytes;
uint32_t bytesRemaining;
uint32_t deviceByteCount;

SPIFI_HANDLE_T *pSpifi;
SPIFI_ERR_T errCode;
static uint32_t buffer[TEST_BUFFSIZE / sizeof(uint32_t)];

/* Report the library version to start with */
libVersion = spifiGetLibVersion();
DEBUGOUT("\r\n\r\nSPIFI Lib Version %02d%02d\r\n", ((libVersion >> 8) & 0xff), (libVersion & 0xff));

/* set the blink rate while testing */
setLedBlinkRate(500);

/* Setup SPIFI FLASH pin muxing (QUAD) */
Chip_SCU_SetPinMuxing(spifipinmuxing, sizeof(spifipinmuxing) / sizeof(PINMUX_GRP_T));

/* SPIFI base clock will be based on the main PLL rate and a divider */
spifiBaseClockRate = Chip_Clock_GetClockInputHz(CLKIN_MAINPLL);

/* Setup SPIFI clock to run around 1Mhz. Use divider E for this, as it allows
higher divider values up to 256 maximum) */
Chip_Clock_SetDivider(CLK_IDIV_E, CLKIN_MAINPLL, ((spifiBaseClockRate / 1000000) + 1));
Chip_Clock_SetBaseClock(CLK_BASE_SPIFI, CLKIN_IDIVE, true, false);
DEBUGOUT("SPIFI clock rate %d\r\n", Chip_Clock_GetClockInputHz(CLKIN_IDIVE));

/* Initialize the spifi library. This registers the device family and detects the part */
pSpifi = initializeSpifi();

/* Get some info needed for the application */
maxSpifiClock = spifiDevGetInfo(pSpifi, SPIFI_INFO_MAXCLOCK);

/* Get info */
DEBUGOUT("Device family = %s\r\n", spifiDevGetFamilyName(pSpifi));
DEBUGOUT("Capabilities = 0x%x\r\n", spifiDevGetInfo(pSpifi, SPIFI_INFO_CAPS));
DEBUGOUT("Device size = %d\r\n", spifiDevGetInfo(pSpifi, SPIFI_INFO_DEVSIZE));
DEBUGOUT("Max Clock Rate = %d\r\n", maxSpifiClock);
DEBUGOUT("Erase blocks = %d\r\n", spifiDevGetInfo(pSpifi, SPIFI_INFO_ERASE_BLOCKS));
DEBUGOUT("Erase block size = %d\r\n", spifiDevGetInfo(pSpifi, SPIFI_INFO_ERASE_BLOCKSIZE));
DEBUGOUT("Erase sub-blocks = %d\r\n", spifiDevGetInfo(pSpifi, SPIFI_INFO_ERASE_SUBBLOCKS));
DEBUGOUT("Erase sub-blocksize = %d\r\n", spifiDevGetInfo(pSpifi, SPIFI_INFO_ERASE_SUBBLOCKSIZE));
DEBUGOUT("Write page size = %d\r\n", spifiDevGetInfo(pSpifi, SPIFI_INFO_PAGESIZE));
DEBUGOUT("Max single readsize = %d\r\n", spifiDevGetInfo(pSpifi, SPIFI_INFO_MAXREADSIZE));
DEBUGOUT("Current dev status = 0x%x\r\n", spifiDevGetInfo(pSpifi, SPIFI_INFO_STATUS));
DEBUGOUT("Current options = %d\r\n", spifiDevGetInfo(pSpifi, SPIFI_INFO_OPTIONS));

/* Setup SPIFI clock to at the maximum interface rate the detected device
can use. This should be done after device init. */
Chip_Clock_SetDivider(CLK_IDIV_E, CLKIN_MAINPLL, ((spifiBaseClockRate / maxSpifiClock) + 1));

DEBUGOUT("SPIFI final Rate = %d\r\n", Chip_Clock_GetClockInputHz(CLKIN_IDIVE));
DEBUGOUT("\r\n");

/* start by unlocking the device */
DEBUGOUT("Unlocking device...\r\n");
errCode = spifiDevUnlockDevice(pSpifi);
if (errCode != SPIFI_ERR_NONE) {
fatalError("unlockDevice", errCode);
}

/* Next erase everything */
DEBUGOUT("Erasing device...\r\n");
errCode = spifiErase(pSpifi, 0, spifiDevGetInfo(pSpifi, SPIFI_INFO_ERASE_BLOCKS));
if (errCode != SPIFI_ERR_NONE) {
fatalError("EraseBlocks", errCode);
}

pageAddress = SPIFLASH_BASE_ADDRESS;
deviceByteCount = spifiDevGetInfo(pSpifi, SPIFI_INFO_DEVSIZE);

/* Enable quad. If not supported it will be ignored */
spifiDevSetOpts(pSpifi, SPIFI_OPT_USE_QUAD, true);

/* Enter memMode */
spifiDevSetMemMode(pSpifi, true);

DEBUGOUT("Verifying device erased...\r\n");
for (idx = 0; idx < deviceByteCount; idx += sizeof(uint32_t)) {
if ( ((uint32_t *) pageAddress)[(idx >> 2)] != 0xffffffff) {
fatalError("EraseDevice verify", SPIFI_ERR_GEN);
}
}
spifiDevSetMemMode(pSpifi, false);

/* fill the buffer with 0x5a bytes */
for (idx = 0; idx < TEST_BUFFSIZE; ++idx) {
((uint8_t *) buffer)[idx] = 0x5a;
}

/* Get the maximum amount we can write and check against our buffer.
If larger, restrict to our buffer size */
loopBytes = spifiDevGetInfo(pSpifi, SPIFI_INFO_PAGESIZE);
if (loopBytes > TEST_BUFFSIZE) {
loopBytes = TEST_BUFFSIZE;
}

pageAddress = spifiGetAddrFromBlock(pSpifi, 0);
bytesRemaining = spifiDevGetInfo(pSpifi, SPIFI_INFO_ERASE_BLOCKSIZE);

/* Write the Sector using the buffer */
DEBUGOUT("Writing Sector 0...\r\n");
while (bytesRemaining) {
if (loopBytes > bytesRemaining) {
loopBytes = bytesRemaining;
}

errCode = spifiDevPageProgram(pSpifi, pageAddress, buffer, loopBytes);
if (errCode != SPIFI_ERR_NONE) {
fatalError("WriteBlock 0", errCode);
}
bytesRemaining -= loopBytes;
pageAddress += loopBytes;
}

/* Get the maximum amount we can write and check against our buffer.
If larger, restrict to our buffer size */
loopBytes = spifiDevGetInfo(pSpifi, SPIFI_INFO_PAGESIZE);
if (loopBytes > TEST_BUFFSIZE) {
loopBytes = TEST_BUFFSIZE;
}

pageAddress = spifiGetAddrFromBlock(pSpifi, 0);

bytesRemaining = spifiDevGetInfo(pSpifi, SPIFI_INFO_ERASE_BLOCKSIZE);

/* Read the sector and validate it using DevRead api*/
DEBUGOUT("Verifying Sector 0...\r\n");
while (bytesRemaining) {
if (loopBytes > bytesRemaining) {
loopBytes = bytesRemaining;
}

errCode = spifiDevRead(pSpifi, pageAddress, buffer, loopBytes);
if (errCode != SPIFI_ERR_NONE) {
fatalError("WriteBlock 0", errCode);
}
/* Read the buffer and make sure it is programmed */
for (idx = 0; idx < loopBytes; ++idx) {
if (((uint8_t *) buffer)[idx] != 0x5a) {
fatalError("Verify block 0", SPIFI_ERR_GEN);
}
}
bytesRemaining -= loopBytes;
pageAddress += loopBytes;
}

/* Done, de-init will enter memory mode */
spifiDevDeInit(pSpifi);

/* indicate test complete serialy and with solid ON led */
DEBUGOUT("Complete.\r\n");
setLedBlinkRate(0);

while (1) {
__WFI();
}

}

Then I run the same code, but with commented erasing and writing functions. When I check the buffer after reading, it is full of 0xFF instead of 0x5A.

static void RunExample(void)
{
uint32_t idx;
uint32_t spifiBaseClockRate;
uint32_t maxSpifiClock;
uint16_t libVersion;
uint32_t pageAddress;
uint32_t loopBytes;
uint32_t bytesRemaining;
uint32_t deviceByteCount;

SPIFI_HANDLE_T *pSpifi;
SPIFI_ERR_T errCode;
static uint32_t buffer[TEST_BUFFSIZE / sizeof(uint32_t)];

/* Report the library version to start with */
libVersion = spifiGetLibVersion();
DEBUGOUT("\r\n\r\nSPIFI Lib Version %02d%02d\r\n", ((libVersion >> 8) & 0xff), (libVersion & 0xff));

/* set the blink rate while testing */
setLedBlinkRate(500);

/* Setup SPIFI FLASH pin muxing (QUAD) */
Chip_SCU_SetPinMuxing(spifipinmuxing, sizeof(spifipinmuxing) / sizeof(PINMUX_GRP_T));

/* SPIFI base clock will be based on the main PLL rate and a divider */
spifiBaseClockRate = Chip_Clock_GetClockInputHz(CLKIN_MAINPLL);

/* Setup SPIFI clock to run around 1Mhz. Use divider E for this, as it allows
higher divider values up to 256 maximum) */
Chip_Clock_SetDivider(CLK_IDIV_E, CLKIN_MAINPLL, ((spifiBaseClockRate / 1000000) + 1));
Chip_Clock_SetBaseClock(CLK_BASE_SPIFI, CLKIN_IDIVE, true, false);
DEBUGOUT("SPIFI clock rate %d\r\n", Chip_Clock_GetClockInputHz(CLKIN_IDIVE));

/* Initialize the spifi library. This registers the device family and detects the part */
pSpifi = initializeSpifi();

/* Get some info needed for the application */
maxSpifiClock = spifiDevGetInfo(pSpifi, SPIFI_INFO_MAXCLOCK);

/* Get info */
DEBUGOUT("Device family = %s\r\n", spifiDevGetFamilyName(pSpifi));
DEBUGOUT("Capabilities = 0x%x\r\n", spifiDevGetInfo(pSpifi, SPIFI_INFO_CAPS));
DEBUGOUT("Device size = %d\r\n", spifiDevGetInfo(pSpifi, SPIFI_INFO_DEVSIZE));
DEBUGOUT("Max Clock Rate = %d\r\n", maxSpifiClock);
DEBUGOUT("Erase blocks = %d\r\n", spifiDevGetInfo(pSpifi, SPIFI_INFO_ERASE_BLOCKS));
DEBUGOUT("Erase block size = %d\r\n", spifiDevGetInfo(pSpifi, SPIFI_INFO_ERASE_BLOCKSIZE));
DEBUGOUT("Erase sub-blocks = %d\r\n", spifiDevGetInfo(pSpifi, SPIFI_INFO_ERASE_SUBBLOCKS));
DEBUGOUT("Erase sub-blocksize = %d\r\n", spifiDevGetInfo(pSpifi, SPIFI_INFO_ERASE_SUBBLOCKSIZE));
DEBUGOUT("Write page size = %d\r\n", spifiDevGetInfo(pSpifi, SPIFI_INFO_PAGESIZE));
DEBUGOUT("Max single readsize = %d\r\n", spifiDevGetInfo(pSpifi, SPIFI_INFO_MAXREADSIZE));
DEBUGOUT("Current dev status = 0x%x\r\n", spifiDevGetInfo(pSpifi, SPIFI_INFO_STATUS));
DEBUGOUT("Current options = %d\r\n", spifiDevGetInfo(pSpifi, SPIFI_INFO_OPTIONS));

/* Setup SPIFI clock to at the maximum interface rate the detected device
can use. This should be done after device init. */
Chip_Clock_SetDivider(CLK_IDIV_E, CLKIN_MAINPLL, ((spifiBaseClockRate / maxSpifiClock) + 1));

DEBUGOUT("SPIFI final Rate = %d\r\n", Chip_Clock_GetClockInputHz(CLKIN_IDIVE));
DEBUGOUT("\r\n");

/* start by unlocking the device */
DEBUGOUT("Unlocking device...\r\n");
errCode = spifiDevUnlockDevice(pSpifi);
if (errCode != SPIFI_ERR_NONE) {
fatalError("unlockDevice", errCode);
}

/* Next erase everything */
/*DEBUGOUT("Erasing device...\r\n");
errCode = spifiErase(pSpifi, 0, spifiDevGetInfo(pSpifi, SPIFI_INFO_ERASE_BLOCKS));
if (errCode != SPIFI_ERR_NONE) {
fatalError("EraseBlocks", errCode);
}*/

pageAddress = SPIFLASH_BASE_ADDRESS;
deviceByteCount = spifiDevGetInfo(pSpifi, SPIFI_INFO_DEVSIZE);

/* Enable quad. If not supported it will be ignored */
spifiDevSetOpts(pSpifi, SPIFI_OPT_USE_QUAD, true);

/* Enter memMode */
spifiDevSetMemMode(pSpifi, true);

/*DEBUGOUT("Verifying device erased...\r\n");
for (idx = 0; idx < deviceByteCount; idx += sizeof(uint32_t)) {
if ( ((uint32_t *) pageAddress)[(idx >> 2)] != 0xffffffff) {
fatalError("EraseDevice verify", SPIFI_ERR_GEN);
}
}*/
spifiDevSetMemMode(pSpifi, false);

/* fill the buffer with 0x5a bytes */
for (idx = 0; idx < TEST_BUFFSIZE; ++idx) {
((uint8_t *) buffer)[idx] = 0x5a;
}

/* Get the maximum amount we can write and check against our buffer.
If larger, restrict to our buffer size */
loopBytes = spifiDevGetInfo(pSpifi, SPIFI_INFO_PAGESIZE);
if (loopBytes > TEST_BUFFSIZE) {
loopBytes = TEST_BUFFSIZE;
}

pageAddress = spifiGetAddrFromBlock(pSpifi, 0);
bytesRemaining = spifiDevGetInfo(pSpifi, SPIFI_INFO_ERASE_BLOCKSIZE);

/* Write the Sector using the buffer */
DEBUGOUT("Writing Sector 0...\r\n");
while (bytesRemaining) {
if (loopBytes > bytesRemaining) {
loopBytes = bytesRemaining;
}

//errCode = spifiDevPageProgram(pSpifi, pageAddress, buffer, loopBytes);
if (errCode != SPIFI_ERR_NONE) {
fatalError("WriteBlock 0", errCode);
}
bytesRemaining -= loopBytes;
pageAddress += loopBytes;
}

/* Get the maximum amount we can write and check against our buffer.
If larger, restrict to our buffer size */
loopBytes = spifiDevGetInfo(pSpifi, SPIFI_INFO_PAGESIZE);
if (loopBytes > TEST_BUFFSIZE) {
loopBytes = TEST_BUFFSIZE;
}

pageAddress = spifiGetAddrFromBlock(pSpifi, 0);
bytesRemaining = spifiDevGetInfo(pSpifi, SPIFI_INFO_ERASE_BLOCKSIZE);

/* Read the sector and validate it using DevRead api*/
DEBUGOUT("Verifying Sector 0...\r\n");
while (bytesRemaining) {
if (loopBytes > bytesRemaining) {
loopBytes = bytesRemaining;
}

errCode = spifiDevRead(pSpifi, pageAddress, buffer, loopBytes);
if (errCode != SPIFI_ERR_NONE) {
fatalError("WriteBlock 0", errCode);
}
/* Read the buffer and make sure it is programmed */
for (idx = 0; idx < loopBytes; ++idx) {
if (((uint8_t *) buffer)[idx] != 0x5a) {
fatalError("Verify block 0", SPIFI_ERR_GEN);
}
}
bytesRemaining -= loopBytes;
pageAddress += loopBytes;
}

/* Done, de-init will enter memory mode */
spifiDevDeInit(pSpifi);

/* indicate test complete serialy and with solid ON led */
DEBUGOUT("Complete.\r\n");
setLedBlinkRate(0);

while (1) {
__WFI();
}
}

Thank you so much for help.

0 项奖励
回复

3,023 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi Jan Hakl,

Please refer to the user guide for checking.
Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------