LPC1837: USB Keyboard/Mouse device updating report

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC1837: USB Keyboard/Mouse device updating report

1,476 次查看
gvk51
Contributor III

Hi All,

I am working on LPC1837 based development board, with "lpcopen_2_18_lpcxpresso_nxp_lpcxpresso_1837" SDK as start point. I am working on examples "usbd_rom_hid_keyboard" & "usbd_rom_hid_mouse" they work fine as USB keyboard/mouse device to host machine.

I see from the below logic of the code

pastedImage_1.png

even if the g_keyBoard.report is empty it is still writing to endpoint, this is creating a continuous stream of packets to host machine, I observed this using Bus-Hound software. Please give your inputs and how to fix this. I would like to send report only if valid data is present.

Thanks & Regards,

Vamshi G.

标签 (3)
0 项奖励
回复
2 回复数

1,240 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi vamshi krishna,

Thank you for your interest in NXP Semiconductor products and 
the opportunity to serve you.

You can add  the function to detect whether report changes between the Keyboard_UpdateReport() and  USBD_API->hw->WriteEP(g_keyBoard.hUsb, HID_EP_IN, &g_keyBoard.report[0], KEYBOARD_REPORT_SIZE), if report keep same you can ignore the  USBD_API->hw->WriteEP(g_keyBoard.hUsb, HID_EP_IN, &g_keyBoard.report[0], KEYBOARD_REPORT_SIZE), otherwise, execute it.

Hope it helps.
Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,240 次查看
gvk51
Contributor III

Hi jeremyzhou,

I tried the mechanism as you mentioned, I believe there is some issue in USB ROM driver. once key is pressed, a report with key event is sent, after that I see its keep on sending the same event even if the keyboard report entries (g_keyBoard.report[]) are zero.

kbd_event_test.png

Please give your inputs.

Thanks & Regards,

Vamshi G.

0 项奖励
回复