LPC1833JBD144 JTAG 无法连接

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC1833JBD144 JTAG 无法连接

1,171 Views
9218sky
Contributor II

您好,自己做了个最小系统板,电路如附件中,其余  IC PIN  NC。MDK 下设置 DEBUG 项,通过ULINK2无法检测到 LPC1833JBD144,帮我查看下附件的电路图是否有问题?另外,能否给我一份 LPC1833JBD144 的最小系统原理电路图?谢谢。

Labels (2)
0 Kudos
1 Reply

1,014 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,

Please check the sch of the LPCXpresso18S37, and refer to it for details.

http://www.nxp.com/assets/downloads/data/en/schematics/LPCX43xx_18xx_V3_Schematic_Rev-B.pdf
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos