LPC1812 TFBGA100 SDRAM

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC1812 TFBGA100 SDRAM

1,629 次查看
otsl
Contributor III

The user manual seems to indicate that you can use the EMC with SDRAM in the 100-pin package (it contains all required dynamic signals), however AN11508 says that the chips only support 16/32 bit SDRAM devices.  Any guidance on using the 8-bit data bus on the TFBGA100 for SDRAM?  Configurations for DYNAMICCONFIG0-1?

标签 (3)
0 项奖励
回复
2 回复数

1,507 次查看
otsl
Contributor III

Hi Sabina.  I had noticed that post, but it didn't really answer my questions.  I can electrically connect the SDRAM to the LPC1812, but how should the EMC be configured?  What DYNAMICCONFIG[0:1] address map setting do I use?  How does the memory mapping work with only an 8-bit external data bus? What happens during a 32-bit write to the mapped area?

0 项奖励
回复

1,507 次查看
Sabina_Bruce
NXP Employee
NXP Employee

Hello,

This community post refers to your question. It is using an LPC43xx, however the AN11508 is for both of these as their EMC modules are the same. 

Please let me know if you have follow up questions. I'll be glad to help you.

Have a nice day!

Sabina

0 项奖励
回复