LPC17xx serial number format

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC17xx serial number format

2,412 次查看
tomaskrysl
Contributor I

Hello,

has the serial number of the LPC uC some format?

In our case, we need to distinguish between LPC1766 and LPC1768 (these devices are identical except for FLASH size).

What I read through IAP call is eg. F50020C7 5A675E1A AF258887 1401000D

Have those numbers some specific meaning?

Thank you

标签 (1)
0 项奖励
回复
3 回复数

2,351 次查看
tomaskrysl
Contributor I

Ok, I've found there is IAP command called "Read part identification number" with IAP command code 5410. However, due to specific circumstances, we need to distinguish the LPC17xx part without this command. We have only device SN accessible. The question is whether the part ID is somewhere hidden inside of the device SN. When I compare the hex values of part ID and device SN I cannot find any similarities. Any idea?

0 项奖励
回复

2,351 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Tomas,

Yes, as Con Verse said, there is no relationship between part ID and serial number.

Regards,

Alice

0 项奖励
回复

2,351 次查看
converse
Senior Contributor V

You must use IAP command 54 - Read part id number. AFAIK, there is no relationship between part ID and serial number.

0 项奖励
回复