LPC178x: UART 38400bps with 12MHz IRC

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC178x: UART 38400bps with 12MHz IRC

422 Views
giusloq
Contributor III

I need to create a RS485/UART communication link between LPC178X and SAMD20 MCU. The communication should be 38400bps.

The clock on SAMD20 is based on an external 32.768kHz crystal (XOSC32K) and DFLL in closed loop mode.

I'm wondering if it is possible to clock LPC178X with internal IRC 12MHz oscillator. The datasheet reports a precision of 1% (11.88-12.12MHz) over all the voltages and temperatures. It seems sufficient for UART communication that usually needs a maximum of 2% error.

Labels (1)
0 Kudos
Reply
1 Reply

396 Views
Habib_MS
NXP Employee
NXP Employee

Hello @giusloq,
I understand that you would use the IRC as core source clock, it is possible, as mentioned in the chapter 1.2 called "Features", as shown in the next image:

Habib_MS_0-1744146716879.png


Also, if you experience any issue do not hesitate to let me know
BR
Habib.

0 Kudos
Reply