LPC1788 WITH 10.1" TFT LCD VIA LVDS INTERFACE

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC1788 WITH 10.1" TFT LCD VIA LVDS INTERFACE

2,303 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by panneerrajan on Mon Mar 10 04:09:15 MST 2014
Hi,

We have used LPC2478 with 4.3 & 7” TFT LCD with touch screen through RGB Interface (8*3= 24BIT).
In future we have to use LPC2478/LPC1788 with 10.1” TFT LCD with touch screen. The 10.1” LCD has 18 bit with LVDS interface.
How to interface the LPC2478/LPC1788 with 10.1” TFT LCD via LVDS interface?
Kindly give me the suggestion for the same
Labels (1)
0 Kudos
Reply
3 Replies

1,766 Views
some1inct
Contributor I

I know this is old but maybe it will help somebody...

You can use TI's DS90C383B LVDS Xmitter for 24-bit color.

I use the DS90C363B for 18-bit displays for RGB565 (16-bit color). 

0 Kudos
Reply

1,766 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by vvijayan75 on Fri Jul 25 04:05:07 MST 2014
hi panneerrajan,
                            you said you worked in 10.1" TFT LCD .MAY I know the value for hsync,vsync,and pulse width for horizontal /vertical?
can you help me to how to make work TFT lcd ?in which manner you wrote a driver for TFT ?
0 Kudos
Reply

1,766 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Martin84 on Mon Mar 10 07:28:49 MST 2014
Hi,

you will need an LVDS Transmitter, which is compatible to the Display's LVDS Interface. Then you can use the RGB-Interface of the µC to drive the LVDS Transmitter. Perhaps you find a recommendation for a LVDS Transmitter in the displays datasheet.
0 Kudos
Reply