I have been working on LPC1788's CAN bus. I have no problem, using it in normal mode where I provide an ID and can read the received packets.
I wanted to read all packets on the CAN bus and it seems I have to use "bypass mode" to achieve this. Unfortunately, when I enter bypass mode, I cannot read any data from the CAN bus. I've tried both interrupt and polling modes.
This is the relevant section of the code:
PINSEL_ConfigPin (0, 0, 1);
PINSEL_ConfigPin (0, 1, 1);
//Initialize CAN1
CAN_Init(CAN_1, 500000);
if(normal_mode) //filter mode
{
//Enable Receive Interrupt
CAN_SetAFMode(CAN_NORMAL); //normal filtering mode
CAN_IRQCmd(CAN_1, CANINT_RIE, ENABLE); //receive enable
CAN_IRQCmd(CAN_1, CANINT_FCE, ENABLE); //full interrupt enable
CAN_IRQCmd(CAN_1, CANINT_IDIE, DISABLE); //ID ready interrupt disable (only used for bypassmode)
}
else //bypass mode
{
CAN_SetAFMode(CAN_ACC_BP); //bypass mode get everything
CAN_IRQCmd(CAN_1, CANINT_RIE, ENABLE); //receive enable
CAN_IRQCmd(CAN_1, CANINT_FCE, ENABLE); //full interrupt enable
CAN_IRQCmd(CAN_1, CANINT_IDIE, ENABLE); //ID ready interrupt enable
}
Any help will be much appreciated.
已解决! 转到解答。
Hi hh hosi,
TIC
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi hh hosi,
TIC
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------