LPC1778 - SSP1 works only in Microwire mode!!!

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC1778 - SSP1 works only in Microwire mode!!!

756 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by michcior on Tue Aug 05 00:06:02 MST 2014
Hello,

SSP1, on LPC1778 (don't now other chips from the family) , works only in Microwire mode!
No matter I do (resets, clock, etc), CR0 register for SSP1 keeps bit #5 high, which results in fixing the port to operate in Microwire mode! Two other SSPs (0,2) work fine and can be configured to any modes. 

No description in errata for that. How it is possible, the bug like that was not identified?

Did anybody come across this issue? Weird, the only comment I can have.

Thanks, Regards,
Piotr.


标签 (1)
0 项奖励
回复
1 回复

741 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by xianghuiwang on Fri Aug 15 17:05:00 MST 2014
hi, michcior,

this is weird. The reset state should be SPI. I double checked a lpc1788 chip, it seems to be correct.
I would really check the state when breaking at the reset handler and set in to see what execution changed this setting.
The LPCOpen has sample project for you to try if needed.

regards,
0 项奖励
回复