LPC1778 ADC VREFP

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC1778 ADC VREFP

1,445 次查看
li_x
Contributor I

Hello, I just noticed that we designed LPC1778 ADC VREFP for 3.0V, isolated and separated from VDDA 3.3V, but in LPC1778 datasheet VREFP is defined as " This should be the same voltage as VDDA, but should be isolated to minimize noise and error." Does that means VREFP should be the same voltage LEVEL as VDDA? From UM10470 user manual document, our software engineer pointed another sentence to me that "Measurement range VSS to VREFP (typically 3 V; not to exceed VDDA voltage level)" which looks like to say it's ok that VREFP is 3.0V different from VDDA 3.3V. Please help for a clarification. Thanks.

标签 (1)
0 项奖励
回复
2 回复数

1,357 次查看
Sabina_Bruce
NXP Employee
NXP Employee

Hello Xiaoling,

As per the datasheet for the LPC1788, the VREFP should only be tied to the VDDA pin if you are not using the ADC or DAC module.

If you are then the values may range from  -0.5 to 4.6 V and as you mentioned above it should not exceed the VDDA voltage level. pastedImage_2.png

Essentially if you are using either ADC or DAC module then 3.0V is not a problem in your case.

Best Regards,

Sabina

0 项奖励
回复

1,357 次查看
li_x
Contributor I

Sabina,

Thank you for the reply. It does help.

Xiaoling

0 项奖励
回复