LPC1769 rev B and LPC1769 with CMSIS-DAP rev D1

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC1769 rev B and LPC1769 with CMSIS-DAP rev D1

1,584 Views
ales_svetina
Contributor I

Hello.
I have a problem...
I have two LPCXpresso boards... LPC1769 REV B and LPC1769 with CMSIS-DAP rev D1
Program I am using is LPCXpresso v8.2.2_650.

"LPC1769 REV B" works fine, when in connect "LPC1769 with CMSIS-DAP" and want to start flash, there comes to error ef (34)

Hello.
I have a problem...
I have two LPCXpresso boards... LPC1769 REV B and LPC1769 with CMSIS-DAP rev D1
Program I am using is LPCXpresso v8.2.2_650.

"LPC1769 REV B" works fine, when in connect "LPC1769 with CMSIS-DAP" and want to start flash, there comes to error ef (34)


What should I do?

Thank you for answers


Labels (1)
0 Kudos
Reply
2 Replies

1,367 Views
soledad
NXP Employee
NXP Employee

Hi, 

Could you please try with an ISP reset. Please check the following link: 

ISP Reset over debug 

Have a great day,

Sol

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,367 Views
ales_svetina
Contributor I

I alrerady tried:

- Window > Preferences > LPCXpresso > Redlink Options > Pull ISP on reset

(on LPC-Link 2

- power board, press isp button then press rst button, release rst button

- also tried

1. GND the ISP pin

2. With ISP still pulled to GND, assert RST and release RST

3. Now remove the GND to ISP pin, and start your debug session

still nothing...

V V čet., 17. jan. 2019 ob 23:16 je oseba soledad <admin@community.nxp.com>

napisala:

NXP Community

<https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg>

Re: LPC1769 rev B and LPC1769 with CMSIS-DAP rev D1

reply from soledad

<https://community.nxp.com/people/soledad?et=watches.email.thread> in *LPC

Microcontrollers* - View the full discussion

<https://community.nxp.com/message/1102622?commentID=1102622&et=watches.email.thread#comment-1102622>

0 Kudos
Reply