LPC1768 Unable to receive data from RTL8304MBI PHY

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC1768 Unable to receive data from RTL8304MBI PHY

6,176 Views
DaveRK
Contributor I

Hello,  Hoping to get some advice on establishing a connection on the RMII interface between an LPC1768 and a RTL8304 PHY.  The PHY indicates it is sending data but the GMAC is not generating any interrupts. 

The PHY has 2 network ports that are operating.  I am able to retrieve data from the PHY on the MDIO interface, which indicates the network ports can link up and indicates the MAC is up.  The PHY statistics registers also indicate it is receiving data on the ports and transmitting data to the MCU.

I am currently using the following connections, which I was able to get to work on a different MCU and this PHY.

NXP LPC1768

 

Realtek PHY

 

Pin

 

RTL8304MBI

I/O

P1_15 / ENET_REF_CLK

-

REFCLK

O

P1_8 / ENET_CRS

-

TXEN

O

P1_9 / ENET_RXD0

-

TXD_0

O

P1_10 / ENET_RXD1

-

TXD_1

O

P1_4 / ENET_TX_EN

-

CRS_DV

I

P1_0 / ENET_TXD0

-

RXD_0

I

P1_1 / ENET_TXD1

-

RXD_1

I

P1_16 / ENET_MDC

-

MDC

I

P1_17 / ENET_MDIO

-

MDIO

I/O

 

I also tried the following connections, but the IAR debugger crashes as soon as the pins are initialized.  So I have returned to the above connections.

NXP LPC1768

 

Realtek PHY

 

Pin

 

RTL8304MBI

I/O

P1_15 / ENET_REF_CLK

-

REFCLK

O

P1_4 / ENET_TX_EN

-

TXEN

O

P1_0 / ENET_TXD0

-

TXD_0

O

P1_1 / ENET_TXD1

-

TXD_1

O

P1_8 / ENET_CRS

-

CRS_DV

I

P1_9 / ENET_RXD0

-

RXD_0

I

P1_10 / ENET_RXD1

-

RXD_1

I

P1_16 / ENET_MDC

-

MDC

I

P1_17 / ENET_MDIO

-

MDIO

I/O

 

I have initialized the pins as follows:

PINSEL_ConfigPin_17xx(1, 0, 1); // P1.0 - ENET_TXD0
PINSEL_ConfigPin_17xx(1, 1, 1); // P1.1 - ENET_TXD1
PINSEL_ConfigPin_17xx(1, 4, 1); // P1.4 - ENET_TX_EN
PINSEL_ConfigPin_17xx(1, 8, 1); // P1.8 - ENET_CRS
PINSEL_ConfigPin_17xx(1, 9, 1); // P1.9 - ENET_RXD0
PINSEL_ConfigPin_17xx(1, 10, 1); // P1.10 - ENET_RXD1
PINSEL_ConfigPin_17xx(1, 14, 1); // P1.14 - ENET_RX_ER
PINSEL_ConfigPin_17xx(1, 15, 1); // P1.15 - ENET_REF_CLK

// NXP LPC1768 MDIO pins
PINSEL_ConfigPin_17xx(1, 16, 1); // P1.16 - ENET_MDC
PINSEL_ConfigPin_17xx(1, 17, 1); // P1.17 - ENET_MDIO

Looking at the RMII interface with a scope I found the TX_EN, TXD1 and TXD0 are steady around 2V and the CRS, RXD0, RXD1 lines are at 0V.  And the REFCLK is at 50MHz.

For a test I removed the TX_EN, TXD0/1, CRS, RXD0/1 connections and with a scope on the PHY pins I see a repeating pattern about every 10ms which appears to auto negotiation pulses, TX_EN is high during a stream of pulses appearing on TXD0/1.

It appears to me that the PHY is working and attempting to send data to the MCU, but when the MCU is connected the signals are snubbed.  So I also tried changing the pins from mode 0 (default, on-chip pull-up resistor enabled) to mode 2 (neither pull-up nor pull-down resistor enabled).  But still no luck.

Any thoughts or ideas greatly appreciated.

Thanks

 

9-16-2022 - Additional info added

Below are 2 scope captures on Power Up of the PHY TX_EN signal with the PHY receiving packets on one of its ports and transmitting to the MCU over RMII. 

The 1st pic is with the PHY TX_EN Connected to the NXP LPC1768 ENET_CRS, the 2nd one with TX_EN NOT Connected.

PHY TX_EN Connected to NXP1768PHY TX_EN Connected to NXP1768

When the pin is connected to the MCU there is some very strange behavior then continuous pulses from 0-2.2V.

PHY TX_EN not connected to NXP1768PHY TX_EN not connected to NXP1768

As you can see when not connected the signal contains repeating pulses from 0-3.3V

Any idea what is going on? or why the MCU pin connected is causing the signal to be reduced to 2.2V?

I also tried setting the pin functions to GPIO Inputs (function 0) and tested with all the resistor modes, pull-up / repeater / Neither pull-up nor pull-down / pull-down, but get the same results.  Also tested on 4 different boards.

I have other boards with a different MCU working with this PHY, and the same MCU working with other PHY chips using the same connections.  With this MCU the PHY indicates it is up and running and scope captures show it is transmitting, but a connected MCU corrupts the signals.

Again, any suggestions greatly appreciated.  We are starting to go out of our minds on this.

Thanks

Dave

0 Kudos
Reply
8 Replies

6,115 Views
DaveRK
Contributor I

Hello XiangJun,

We do have the connections as you suggested.

DaveRK_0-1663802499882.png

We verified the RTL8304 is sending data to the NXP LPC1768 MCU, but the MCU is not generating RX interrupts.

The Firmware is configured to send ARP packets at a rate of 1/s.  We do see 7us pulses on the MCU TX_EN pin at a rate of 1/s, but there is no activity on the ENET_TXD[1:0] pins.  EMAC TX interrupts do take place.

Is there anything I can look at to get more info?

Thanks

 

0 Kudos
Reply

6,119 Views
DaveRK
Contributor I

Hi XiangJun,

 

Yes, the connections you described are how we have the connections.

DaveRK_0-1663771647699.png

 

0 Kudos
Reply

6,146 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

I think the following connection of Ethernet interface is correct.

 

xiangjun_rong_0-1663644582845.png

The following the ethernet signal timing I copied from data sheet of LPC546xx.

xiangjun_rong_0-1663649708477.png

The ENET_TX_EN is an output signal from the LPC17xx, regarding the 2.2V voltage, what is the VDD(3V3) power supply voltage? the VDD(3V3) voltage is the power supply voltage for the I/O
ports.

Hope it can help you

BR

XiangJun Rong

0 Kudos
Reply

6,139 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

I attach the schematics of LPCXpressoLPC1769 EVK board, pls refer to page three for the Ethernet PHY connection.

Hope it can help you

BR

XiangJun Rong

0 Kudos
Reply

6,127 Views
DaveRK
Contributor I

Thanks for getting back to me XiangJun Rong.

VDD is 3V3.

I understand the connections for the LPCXpressoLPC1769 are TX to TX and RX to RX, however, this connection is to the Microchip LAN8720, which specifies the TX pins as inputs and the RX pins as outputs. 

The chip we are using, the Realtek RTL8304 specifies TX pins as outputs and RX pins as inputs.

Previously, for a test I connected the TX pins to TX (Outputs to Outputs) and RX to RX (Inputs to Inputs), but the MCU would stop operating in the IAR debugger exactly when the pins were configured as RMII pins.

Additionally, we were able to get the RTL8304 working on a different manufacturers MCU with  RTL8304 TX output connected to MCU RX input and RTL8304 RX input connected to MCU TX output.

But, we would like to get it working on the NXP LPC1768.

Unless the NXP LPC1768 RMII pins autodetect inputs/outputs?

Is there something than can explain the scope traces above?

Thanks

0 Kudos
Reply

6,119 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

Based on the pic I copied from RTL4304, I think you should connect as following:

 

xiangjun_rong_0-1663738271999.png

LPC1768                            RTL8304MBI PHY

P1.0-RMII_TXD0                RXD0    pin 22

P1.1-RMII_TXD1                RXD1       pin23

P1.4-RMII_TXEN                CRS_DV   pin21

 

P1.9-RMII_RXD0                TXD0     pin 16
P1.10-RMII_RXD1               TXD1    pin15
P1.8-RMII_CRS                  TXEN     pin17

P1.15-RMII_CLK                  REFCLK   20


P1.16-RMII_MCD               SCL/MDC  pin27
P1.17-RMII_MDIO             SDA/MDIO   pin28

Pls have a check.

BR

XiangJun Rong

 

0 Kudos
Reply

6,086 Views
DaveRK
Contributor I

We finally got it working. 

Using the pin connections we started with: (Outputs -> Inputs)

DaveRK_0-1663938619661.png

If anyone has dealt with Realtek then you know how secretive they are about their documentation.  They will not release documentation or the phy register set. We finally got the spec after signing NDA's.  But no register information.

Then when you finally get the spec after numerous requests you find it is so vague that you have tons of questions.  So you start the question process.  Ask 1 question and you will not get a response.  Ask 10 questions and you will get a single question in return. 

The question from them was usually "what are the contents of register 'x'?"

So, after months of this I get "The contents of that register should be 'y', clear bit 14".

After clearing bit 14 of this register the phy now works.

I asked them what is the function of this bit and why does it need to be cleared.  We did not have to do this when using the phy with a different MCU.

I get in response "The reason should be some RMII pins share with some LED pins"

Sorry for the rant.  Just wanted to warn anyone who has the privilege to work with Realtek, and to let everyone know that has worked with them that I surely felt your pain.

 

0 Kudos
Reply

2,154 Views
goddOnly
Contributor I
I have the same problem, which register is cleared bit 14?
0 Kudos
Reply