LPC1768 UART3 ISSUE Regarding Receiving Side.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

LPC1768 UART3 ISSUE Regarding Receiving Side.

跳至解决方案
1,314 次查看
PK_1114
Contributor II

Dear Sir,

I am using the LPC1768 UART3 PIN0_0,PIN0_1 as TX and RX Transmitting data is working fine but data receiving Interrupt is not working  and also in polling also it not working at that place we place LPC1769 it working fine. (Operating Frequency 90MHz, with Baud rate of (9600 - 115200)bps. Please provide any information regarding it.

Thank You,

B PAVAN KUMAR.

 

 

 

0 项奖励
回复
1 解答
1,308 次查看
EdwinHz
NXP TechSupport
NXP TechSupport

Hello @PK_1114,

I recommend looking into the UART Line Status Register. This register contains error bits that should provide you with a better insight of why the reception interrupt is not working properly on the LPC1768 specifically. Let me know if you identify an error.

 

BR,

Edwin.

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,309 次查看
EdwinHz
NXP TechSupport
NXP TechSupport

Hello @PK_1114,

I recommend looking into the UART Line Status Register. This register contains error bits that should provide you with a better insight of why the reception interrupt is not working properly on the LPC1768 specifically. Let me know if you identify an error.

 

BR,

Edwin.

0 项奖励
回复
1,085 次查看
PK_1114
Contributor II

Hai Sir @EdwinHz ,

 

That LPC1768 IC Batch issue sir, by placing other LPC1768 IC It is working ok sir,

 

Thank You,

B Pavan Kumar

 

0 项奖励
回复