LPC1768: IAP reinvoke results in hard fault

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC1768: IAP reinvoke results in hard fault

Jump to solution
2,095 Views
volkerweber
Contributor II

Hi there,

 

I am trying to use the reinvoke functionaliry of the IAP set on my LPC1768 but it always results in an Hard Fault error (see attached picture). To use the reinvoke feature I do the following as suggested in the manual:

 

__disable_irq();

LPC_SC->PLL0FEED  = 0xAA;   
LPC_SC->PLL0FEED  = 0x55;    
LPC_SC->PLL0CON   = 0;    
LPC_SC->PLL0FEED  = 0xAA;    
LPC_SC->PLL0FEED  = 0x55;    
LPC_SC->CLKSRCSEL = 0;    

unsigned int cmd[5], res[5];    
cmd[0] = 57;  
__set_MSP(*((uint32_t *) 0x1FFF0000));
iap_entry(cmd, res);‍‍‍‍‍‍‍‍‍‍‍‍‍

 

Are there any mandatory steps before trying to use this, e.g. regarding the timing? As I cannot debug the functions inside the boot rom memory area (0x1FFF 0000 - 0x1FFF 1FFF) I do not see how to progress here.

 

Any help is appreciated, thanks in advance

Labels (1)
Tags (2)
0 Kudos
Reply
1 Solution
1,956 Views
volkerweber
Contributor II

I managed to get it to work. Quoting the manual:

It maps boot vectors, sets PCLK = CCLK / 4, configures UART0 pins Rx and Tx, resets TIMER1 and resets the U0FDR (see Section 14.4.12).

In my point of view, that does not include that TIMER1 has to be enabled, however this solves it:

LPC_SC->PCONP |= CLKPWR_PCONP_PCTIM1;‍‍

Perhaps this is also useful for somebody else.

View solution in original post

0 Kudos
Reply
1 Reply
1,957 Views
volkerweber
Contributor II

I managed to get it to work. Quoting the manual:

It maps boot vectors, sets PCLK = CCLK / 4, configures UART0 pins Rx and Tx, resets TIMER1 and resets the U0FDR (see Section 14.4.12).

In my point of view, that does not include that TIMER1 has to be enabled, however this solves it:

LPC_SC->PCONP |= CLKPWR_PCONP_PCTIM1;‍‍

Perhaps this is also useful for somebody else.

0 Kudos
Reply