LPC1765 updating image issue

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC1765 updating image issue

832 次查看
amandachiang
Contributor I

Hi,

Good day.

I have an issue on updating the image of the LPC1765 On The Air(OTA). Pls help to give some advice if practicable. Thanks.

The SSPO of the LPC1765 have been used for the SD card and SPI flash in TDM. The data for OTA will be uploaded through the GPRS. The operation of OTA will be failed when the SD card have not been removed from our device. Even though we have already pulled high the CS# of the SD(SD card can't work when CS pull high). 

Could you help on this. Thank you.

标签 (1)
0 项奖励
回复
1 回复

716 次查看
soledad
NXP Employee
NXP Employee

Hello Amanda,

Please check the below thread and let me know if this helps!

Firmware Over the Air (FOTA) | www.LPCware.com 


Have a great day,
Sole

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复