LPC1549 watchdog period while the boot process

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC1549 watchdog period while the boot process

804 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by ihar on Thu Oct 02 04:41:24 MST 2014
I am going to use LPC1549 part for motor control drivers and upload their firmware by external master controller via CAN bus.
I have read in LPC15xx manual(UM10736) at chapter 5.4 "...If the boot pins are
sampled LOW and the watchdog overflow flag is set, the external hardware request to
start the ISP command handler is ignored..."
How much time does takes watchdog period while bootloader code is executing?
标签 (1)
0 项奖励
回复
0 回复数