LPC1343 on-chip HID driver streaming values

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC1343 on-chip HID driver streaming values

2,262件の閲覧回数
eero_prittinen
Contributor I

Hi,

I am currently building a solution that uses the LPC1343 built in HID USB on-chip driver based on the DALI demo described in application note AN11175. The problem I'm facing is that when I connect the device to a PC and inspect the HID data, it comes as a stream of values instead of a value every time something is available. This means, that when there is no activity on the dali bus and no data is provided to the USB get in report callback, the device will send just zeroes. What I would like to achieve is to only send values over USB when they are available. Is there a way in the on-chip driver to disable the streaming of data and instead set the values available on demand?

ラベル(1)
タグ(3)
0 件の賞賛
返信
1 返信

2,188件の閲覧回数
FelipeGarcia
NXP Employee
NXP Employee

Hi,

 

Unfortunately, the USB HID driver is placed in the boot ROM of the LPC134x, and can’t be changed by the user. Sorry for the inconvenience that this may cause you.

 

Regards,

Felipe

0 件の賞賛
返信