LPC1227 with clevb 663b blueboard.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC1227 with clevb 663b blueboard.

934件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by moonchill on Tue Dec 09 23:11:53 MST 2014
Hi all,

Now i have LPC 1227 connected with the CLEV663B blueboard. I have downloaded the example codes for Polling from website and trying to run it. However, when i debug the code. It shows that .axf file is missing. I have setting the build configuration to Debug 1227 and also choose the correct MCU in property page. Can some1 help me?  Thanks .
ラベル(1)
0 件の賞賛
返信
1 返信

874件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Wed Dec 10 00:47:29 MST 2014
If there is no AXF file to debug, this would generally suggest that the project has failed to build - check the build log for details:

http://www.lpcware.com/content/faq/lpcxpresso/build-console

What version of LPCXpresso are you using? And are you using the latest version of these examples and read the included documentation (I see a new version was posted a few days ago)…

http://www.nxp.com/demoboard/CLEV663B.html#documentation

Note that from a quick look at this eample bundle, you will need to switch all of the library projects to build the LPC1227 debug build configuration in order to successfully build the 1227 configuration of the 'Classic' application.

http://www.lpcware.com/content/faq/lpcxpresso/change-build-config

Finally, note that the CLEV663B board and its examples are produced by a different division within NXP. For support on using the CLEV663B board, I would suggest using the email support link on the left hand side of this page:

http://www.nxp.com/demoboard/CLEV663B.html#support

Regards,
LPCXpresso Support
0 件の賞賛
返信