LPC11U68 ADCs 2Ms/s

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC11U68 ADCs 2Ms/s

699 次查看
bobbann
Contributor I

LPC11U68 ADCs claim to run at 2Ms/s, but I am seeing conversion times of >60 clock cycles at 48MHz (<1Ms/s). I'm running a SeqA with a single channel in Burst mode, with an IRQ handler in RAM reading results into a simple buffer. Can anyone point me at a code sample which can achieve the 2Ms/s. I've checked the clock divider is 0 and Vdda is 3.3V.

Cheers, Bob.

EDIT :

  I solved this issue using DMA. 2MHz was then achievable.

标签 (1)
标记 (3)
0 项奖励
回复
1 回复

554 次查看
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Bob,

    Thank you for your problem solutions sharing!


Have a great day,
Jingjing

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复