LPC11U37H debugging not possible as no emulator is shown

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

LPC11U37H debugging not possible as no emulator is shown

跳至解决方案
1,243 次查看
nxp87599
NXP Employee
NXP Employee

Fresh LPC11U37H just taken out of the box. Connected to the PC via USB cable to J6 on LPC board.

Windows device manager shows: LpcDevice.

Downloaded IOH software package from website, imported in LPCXpresso 8.0.0 Build 526, build sample project "nxp_lpcxpresso_11u37h_ioh_uart" and tried to debug it. During looking for a connected emulator the entry in the Windows device manager changes from LpcDevice to "LPC-LinkII UCom Port" in section "Ports". However, there is no CMSIS-DAP and the list of found emulator is empty.

Any idea which driver might be missing or what else needs to be done?

0 项奖励
回复
1 解答
1,162 次查看
nxp87599
NXP Employee
NXP Employee
0 项奖励
回复
1 回复
1,163 次查看
nxp87599
NXP Employee
NXP Employee

This description solved my issue: https://community.nxp.com/thread/389044  .

0 项奖励
回复