LPC11C24 reinvoking the ISP on CAN systems using bitrates unequal 100k

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC11C24 reinvoking the ISP on CAN systems using bitrates unequal 100k

1,037件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by mhg on Mon Dec 08 02:24:03 MST 2014
The old thread started with "ISP -> APP" and ended on "APP -> ISP" and bitrate issues. Following R2D2s suggestion "Please start a new thread, this one is old and long enough..." i start this new thread.

The problem: Reinvoking the ISP from application code results in 100k bit rate on CAN. Doing this in systems with different CAN BTR setting will fail.

Solutions discussed:
1. Turn all other nodes off or switch all of them to 100k before.
=> This is often not possible running systems with third party components off-the-shelf.
2. Reimplement the on-chip ROM code to replace the CAN BTR setting.
=> Huge coding effort just for adjusted BTR settings.

R2D2 pointed on two interesting details:
1. The "reinvoke ISP" command of the IAP on LPC15 is providing a parameter to select the interface (see thread).
2. R2D2 wrote: "... but it's also useful to switch from IRC to crystal Wink. Note: That's no theory, that's really working".

@1) Is there something (undocumented) similar for BTR setting on LPC11 ?
@2) On my LPC11C24 reinvoking the ISP is always resulting in 100k regardless of the oscillator settings. Is there any special trick?

User manual 26.3.8.1:
3.) A pattern at 0x0000 02FC is used to disable ISP.

@3) Is there any other undocumented magic number (e.g. for BTR setting)?

Reimplementing the on-chip ROM code (with relocation to RAM etc.) appears to me not so pleasant.

Are there any tricks known, that may enable ISP operation at other bitrates?
ラベル(1)
0 件の賞賛
返信
0 返答(返信)