LPC11C24 - Second bootloader and target application with CAN phy support

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC11C24 - Second bootloader and target application with CAN phy support

557 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by bomba82 on Wed Feb 05 02:24:23 MST 2014
After opening a thread for HardFault problems caused by CAN phy, I think that I have to know something in advance.

Does someone know if it's possible to develop a target application with CAN phy support, that can be deployed to the device via a second bootloader with CAN phy support?
I think my second bootloader is already ok, but I can't have success in developing a running target application. As I can understand the problem is that the CAN ISR is the cause of some kind of problem.

Can someone from NXP tell if it's impossible to implement that solution? And in that case, what's the reason?
标签 (1)
0 项奖励
回复
0 回复数