LPC SIGTRAP error "Break at address with no debug information..."

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC SIGTRAP error "Break at address with no debug information..."

1,607 次查看
swetha_v
NXP Employee
NXP Employee

After changing the I/O in an example project running on a board that uses the LPC55S66JBD100 and starting the debug session, the following SIGTRAP error occurs. What could cause this error? Issue with the code or the debugger configuration?

error_log.PNG

Thanks.

标签 (1)
0 项奖励
回复
2 回复数

1,558 次查看
converse
Senior Contributor V

Looks like it is possibly stack corruption. When you say "Changing the I/O" what do you actually mean - what, exactly, did you change?

0 项奖励
回复

1,558 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Swetha,

Thank you for contacting us.

First we need to identify the problem is on project or IDE system.

Please create a NEW workspace and import a NEW demo code ( for example led blink demo), see if the problem exists? if no issue, import your working project into this new workspace, how is the connecting?


Have a great day,
Jun Zhang

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复