LPC 43S67 and GainSpan GS2100M sdio adapter board

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC 43S67 and GainSpan GS2100M sdio adapter board

1,498件の閲覧回数
omidathari
Contributor II

Hello

I've got your LPCXpresso43xx/18xx with OM13082 and a GainSpan SDIO Wifi Adapter Board GS2100M.

I get an error when I run the example app from lpc_open "periph_sdio"

DBG: SDIO Card init error: 0xFFFFFFFE, -2

Any help is appreciated

Omid 

ラベル(2)
0 件の賞賛
返信
2 返答(返信)

1,252件の閲覧回数
omidathari
Contributor II

The sd/mmc socket on the OM13082 is not connected to vcc.

0 件の賞賛
返信

1,252件の閲覧回数
soledad
NXP Employee
NXP Employee

Hello Omid,

On the LPC4337 Xpresso shield board JP3 must be soldered to shunt, could you please double check this configuration?


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信