Keil MDK 5.29 can't download to LPCXpresso55S69-EVK

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Keil MDK 5.29 can't download to LPCXpresso55S69-EVK

2,131 Views
michael_t_check
Contributor I

It's a rev A1 board. The same project downloads just fine with MCUXpresso IDE v11.1.1 [Build 3241] [2020-03-02].

Clearly the debugger setup routines in "NXP.LPC55S69_DFP.pdsc" need to be updated.

Here's the trace from Keil:

Load "debug\\hello_world.out"
Info: LPC55xx connect srcipt start
Info: APIDR: 0x002A0000
Info: DPIDR: 0x6BA02477

File : C:\Keil_v5.29\Arm\Packs\NXP\LPC55S69_DFP\12.1.1\NXP.LPC55S69_DFP.pdsc
Sequence : DebugPortStart -> EnableDebugMailbox
Context : Item #0: <block>::Line 29
Expression : "v5.29\Arm\Packs\NXP\LPC55S69_DFP\12.1.1\NXP.LPC55S69_DFP.pdsc"
E310 : Debug access failed - cannot read AP register 0x00000008 (AP '0x00000002'))

Cannot access Memory (@ 0x00000000, Write, Acc Size: 4 Byte)
Error: Flash Download failed - Target DLL has been cancelled
Flash Load finished at 23:16:30

Labels (1)
0 Kudos
Reply
1 Reply

2,050 Views
Sabina_Bruce
NXP Employee
NXP Employee

Hello Michael,

Hope you are doing well.

Could you please try the recommendation posted on this thread.

https://community.nxp.com/thread/514830 

Best Regards,

Sabina

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

----------------------------------------------------------------------------------------------------------------------- 

0 Kudos
Reply