Jump to ISP bootloader from application mode

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Jump to ISP bootloader from application mode

跳至解决方案
3,675 次查看
tks11111
Contributor II

Hi,

Is there a way to jump to ISP bootloader mode from application mode without pressing the ISP button?

I tried the method mentioned in Entering ISP mode from application code in LPC55 - NXP Community, but none can force the LPC5528 and LPC55S28 into ISP mode.

My IC Device ID is 0xA010111C and 0xA010119C.

Let me know if there is anything I need to provide.

Thanks.

标签 (2)
标记 (1)
0 项奖励
回复
1 解答
3,439 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @tks11111 

1) "We added a capacitor between pin0_5 and GND, and set pin0_5 to digital low before we reset the IC.
After doing this, the IC could enter ISP boot mode after the reset."

->> This is use  ISP pin entered ISP mode.

2)Pull up PIO0_5 is when using code jump. While I haven't test on my side, because there is no chip with code 1927 on my side. Just other customer's experience. You can test.

 

BR

Alice

在原帖中查看解决方案

0 项奖励
回复
9 回复数
3,648 次查看
tks11111
Contributor II

Hi Alice,

The date code is 1927.

I also tried the method you provided, but the chip kept resetting and could not enter ISP mode.

Do I need to erase the app code before calling NVIC_SystemReset?

 

BR,

Peter

 

 

0 项奖励
回复
3,568 次查看
nxf64834
NXP Employee
NXP Employee

Hi,

Please refer below snippet from Errata for tried and tested method to enter ISP mode from application.

nxf64834_0-1705394992581.png

Thanks.

0 项奖励
回复
3,511 次查看
tks11111
Contributor II

Hi,

As we discussed previously, I tried this method and it did not work.

That is why I asked for another method to enter ISP mode from the application.

The workaround method I used was to wire a capacitor between P0_5 and GND, and set P0_5 to digital low before I called NVIC_SystemReset(). This way, the IC detected P0_5 low and entered ISP mode.

However, this method had some flaws because we might need to add a capacitor and wait for the discharge time.

I wonder if there is any method that can enter ISP mode without adding any components.

Thanks.

 

BR,

Peter 

0 项奖励
回复
3,613 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @tks11111 

I don't think need erase code.

Could you please first use ISP pin to test, whether your chip can enter ISP mode successfully, and can communication with PC through UART port or USB?

 

BR

Alice

0 项奖励
回复
3,586 次查看
tks11111
Contributor II

Hi Alice,

I can enter ISP mode on my chip by using the ISP pin. I also use USB1 as a communication port with my PC.

After the chip enters ISP mode, the PID/VID changes.I use the blhost tool to upload my FW bin file, and the chip works correctly after it returns to app mode."

 

BR,

Peter

0 项奖励
回复
3,572 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @tks11111 

How about have a pullup resistor connected to the P0_5 pin ?

https://community.nxp.com/t5/LPC-Microcontrollers/LPC5526-run-isp-bootloader/m-p/1609563  

 

BR

Alice

0 项奖励
回复
3,561 次查看
tks11111
Contributor II
Hi Alice,
We added a capacitor between pin0_5 and GND, and set pin0_5 to digital low before we reset the IC.
After doing this, the IC could enter ISP boot mode after the reset.
I wonder if pullup resistor can have the same result?

BR,
Peter
0 项奖励
回复
3,440 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @tks11111 

1) "We added a capacitor between pin0_5 and GND, and set pin0_5 to digital low before we reset the IC.
After doing this, the IC could enter ISP boot mode after the reset."

->> This is use  ISP pin entered ISP mode.

2)Pull up PIO0_5 is when using code jump. While I haven't test on my side, because there is no chip with code 1927 on my side. Just other customer's experience. You can test.

 

BR

Alice

0 项奖励
回复
3,662 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @tks11111 

What is the date code of your device? You can find on marking of your chip.

And there is issue with  date code 2101 (yyww) onward, detail:

https://www.nxp.com.cn/docs/en/nxp/errata/LPC55S2x_LPC552x_ES.pdf 

Alice_Yang_0-1704879593141.png

 

BR

Alice

 

0 项奖励
回复