Issue: The fsl_power driver is missing in the project. Error when configuring ADC on LPC845

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Issue: The fsl_power driver is missing in the project. Error when configuring ADC on LPC845

2,198 Views
tomchr
Contributor III

Hello,

I'm trying to use the ADC on an LPC845. I've done so successfully in the past with an older version of the IDE and SDK. With the latest version I get an error saying that the fsl_power driver is missing.

I can right click on the error. That gives me this option: "Add component power_no_lib into the project". That doesn't work.

fsl_power.h and fsl_power.c are in the driver directory and I #include "fsl_power.h" without issues. The power driver is also selected in the SDK configuration.

I hope someone can shine some light on what's going on and how to fix it.

Tom

0 Kudos
Reply
4 Replies

2,091 Views
tomchr
Contributor III

Will do. Thank you.

0 Kudos
Reply

2,180 Views
tomchr
Contributor III

I've tried creating a new project. I made sure to enable the ADC and power drivers in the project setup. I still get the "fsl_power driver is missing" error.

Basically it's not possible to configure the ADC using the peripheral configuration tool.

Is there a way to get MCUxpresso to recognize fsl_power and link it correctly?

Tom

0 Kudos
Reply

2,064 Views
ZhangJennie
NXP TechSupport
NXP TechSupport
0 Kudos
Reply

2,122 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi @tomchr 

Please use the previous version as workaround for the moment.

I have reported this issue internally. 

I will keep you informed if any update.

Thanks,

Jun Zhang