Is there any tutorial on how to use LPC Link-2?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Is there any tutorial on how to use LPC Link-2?

2,448 次查看
vxs187
Contributor III

I am new to operating an LPC MC, would like to know if there is any shortcut route to using this, I am not an Embedded programmer, would like to know if there is any course that I might be able to do in order to get an insight on programming the MC and being able to use the same in a project. 

标签 (1)
2 回复数

1,958 次查看
soledad
NXP Employee
NXP Employee

Hi,

I suggest you to check the following custom blog

https://mcu-things.com/blog/how-to-use-lpc-link2/ 

In addition please check the following videos:

LPC-Link 2 Debugger - YouTube 

LPC Tips & Tricks: LPCScrypt LPC-Link2 Debug Probe Programming - YouTube 

LPC-Link 2 Debug Adapter Extends LPCXpresso Ecosystem - YouTube 

Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,958 次查看
vxs187
Contributor III

Hi Sol,

I am using the UART TX to transmit messages to a computer through an Arduino, I guess the data rate of Link-2 is way higher than the data rate of the Arduino. I am not sure of it though, could you help me with this? 

0 项奖励
回复