Is the LPC2478 Input/Output have builin sch-mitt trigger?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Is the LPC2478 Input/Output have builin sch-mitt trigger?

1,224 次查看
sureshpandi
Contributor I

Hi,

As per LPC2478 data sheet the I/O have builtin sch-mitt trigger.

Is really LPC2478 Input/Output have builtin sch-mitt trigger? (attached the screen shot)

Please confirm.

标签 (2)
0 项奖励
回复
1 回复

1,097 次查看
CarlosCasillas
NXP Employee
NXP Employee

Hi Pandi,

The built-in Schmitt Triger circuitry is the regular circuit for digital IO. Based on the image that you sent, it just applies to the Digital Input, as the Digital Output and Analog Inputs are on separate routes.

You could check the hysteresis voltage (Vhys) on Table 9 “Static characteristics” of LPC2478 Datasheet, available on the following link:

http://www.nxp.com/docs/en/data-sheet/LPC2478.pdf


Hope this will be useful for you.
Best regards!
/Carlos
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复