Invalid Checksum of first 512 UU-encoded bytes

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Invalid Checksum of first 512 UU-encoded bytes

1,624 Views
bilalqureshi_ep
Contributor II

Hi,

I have made a UU-encoding console application in c# and used flashMagic tool as reference to confirm if i am doing everything right. I need it to write on LPC1767 microcontroller. The only issue i am facing is that the checksum of first 512 bytes are not valid, what i am getting is 34964 whereas what flashmagic provides is 35644, according to 

http://www.nxp.com/docs/en/application-note/AN11229.pdf the raw hex is to be added with each other to make a valid checksum, but in my case only first checksum is not valid rather then this all the checksums are valid. As i am new to this field i need to know where i am wrong and how will i be able to fix it.

First 512 bytes are

:10000000502F082011020000190200001B020000FE
:100010001D0200001F02000021020000000000007D
:1000200000000000000000000000000023020000AB
:10003000250200000000000027020000A14F01007F
:100040002B020000ED53010001540100B9540100DE
:10005000CD550100C95901000D5A0100195A01007E
:10006000315A01002B020000A13E000001410000B6
:10007000194300002B0200002B0200002B0200009D
:100080002B020000492C01002B0200002B02000073
:100090002B0200002B0200002B0200002B020000AC
:1000A0002B0200002B0200002B0200002B0200009C
:1000B0002B0200002B0200002B0200002B0200008C
:1000C0002B0200002B0200002B02000000F002F8BF
:1000D00000F060F80AA090E8000C82448344AAF182
:1000E0000107DA4501D100F055F8AFF2090EBAE880
:1000F0000F0013F0010F18BFFB1A43F0010318475C
:1001000058200400982004000A444FF0000C10F816
:10011000013B13F0070408BF10F8014B1D1108BF85
:1001200010F8015B641E05D010F8016B641E01F825
:10013000016BF9D113F0080F1EBF10F8014BAD1C75
:100140000C1B09D16D1E58BF01F801CBFAD505E093
:1001500014F8016B01F8016B6D1EF9D59142D6D3ED
:10016000704700000023002400250026103A28BF15
:1001700078C1FBD8520728BF30C148BF0B60704719
:100180001FB59DE8030000F0A5FA00F0CEF81FBDF2
:1001900010B510BD00F046FB1146FFF7F1FF1DF052
:1001A0002DFF00F064FB03B4FFF7F2FF03BC00F087
:1001B00091FB000006480000D0F800D00548064A30
:1001C00012681047E07F0010F11FFF1F3900000088
:1001D000C4010000CC010000C80100000B49D1F8A7
:1001E00000C04A685CF8043B1068184442F8040BED
:1001F0008C4528BFA1F1DC0C8A4228BFA1F1DC02AA

Thank You,

Regards,

M.Bilal

Labels (1)
0 Kudos
Reply
1 Reply

1,289 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi

I suggest following the AN 5.3  Writing to RAM section, take use the command from AN to test if the system can work as expected. thus we can verify if the system functions well with checksum

pastedImage_1.png

Data is sent and received in UUencoded format .  The chip is only recogonized the checksum that is generated by adding raw data (before UU-encoding) bytes.

Regarding how the FlashMagic handle checksum inside, we would suggest you contact Welcome - EmSA  who is FlashMagic producer and their forum:

Flash Magic Forum - Index 


Have a great day,
Jun Zhang

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply