Interfacing an monochrome STN-Display with T6963C or SED1335 to LPCxxxx LCD-Controller

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Interfacing an monochrome STN-Display with T6963C or SED1335 to LPCxxxx LCD-Controller

931 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Martin84 on Mon Feb 03 06:37:22 MST 2014
Hi,

does anyone have experience in driving monochrome STN-Displays with T6963C or SED1335-Controller and the internal LPCxxxx LCD-Controller?

When I'm using the external LCD-Controller (for example the T6963C) I have to use GPIOs or Adress- and Data-Lines. What should I do when I want to use the LCD-Controller of the LPCxxxx (for example LPC4357) ? Do I have to bypass the T6963C Controller and drive the signals FLM, CL1, CL2,... directly?

Is there a application note or an example how to do this?

Regards,

Martin 
Labels (1)
0 Kudos
Reply
0 Replies