ISP programming of LPC1225FBD64/301 - autobaud failure issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ISP programming of LPC1225FBD64/301 - autobaud failure issue

1,240 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by neelamnaik on Wed Apr 22 22:36:50 MST 2015
I am using LPC1225FBD64 in my project.  Using flash magic V9.000 to program using ISP.
For the very first time we tried to connect and it did connect, but mistakenly we loaded the hex file generated from AN11069 and  then onwards I am not able to connect/communicate with the IC using ISP ( flash magic).
Tried to connect using different baud as 9600 to 57600,
tried to connect by giving LOW on RESET pin

I am holding the pin PIO0_12 low and powering the device but when trying to connect using flash magic I am getting error as :

failed to autobaud .....

please help.

Also, found below statement in User manual, want to know more details about the same:

"If PIO0_12 is sampled low and the watchdog overflow flag is set, the external hardware
request to start the ISP command handler is ignored."
my query is how to know if " the watchdog overflow flag  is set " ? and whether this could be reason of my issue of failing to autobaud ?

please help as i am stuck in this issue.
regards,
neelam


Labels (1)
0 Kudos
Reply
2 Replies

1,172 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by neelamnaik on Thu Apr 23 22:44:53 MST 2015
Hi,
Thanks for the feedback.. The issue is solved.
The ISP entry pin was not set properly..

Regards,
Neelam
0 Kudos
Reply

1,172 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by nerd herd on Thu Apr 23 10:25:32 MST 2015
Hi neelamnaik,

Just to rule out some factors, have you tried using a different PC to see if there is any difference in behavior? Have you hooked an oscilloscope or logic analyzer to see the data being sent over UART?
0 Kudos
Reply