IEC60335 certificate

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

IEC60335 certificate

1,428 次查看
tomi
Contributor I

we are using LPC1768 in a safety project.

there is a Application Note AN10918 for IEC60335 Class B certified library  

where can i find the certificate for this library

Thanks for help

Thomas

标签 (2)
0 项奖励
回复
2 回复数

1,280 次查看
arunt
Contributor I

Does the LPC800 have a library for IEC60355?

0 项奖励
回复

1,280 次查看
soledad
NXP Employee
NXP Employee

Hi,

Please check the Sec_121512 doc attached. 

Have a great day,
Sol

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复