ICP programmer for LPC9xxx

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ICP programmer for LPC9xxx

3,934 Views
grgsaliba
Contributor I

I've come across an old board with the LPC9361 which I need to re-program. The interface available is ICP but I am not sure which programmer I need. All online searches point to the FDI USB-ICP-LPC9xx but this has long been obsolete. Is there any current programmer that can do ICP programming on the LPC9361 ?

Note: removing the chip from the board is not an option and only the ICP interface is available.

Tags (1)
0 Kudos
Reply
4 Replies

2,660 Views
8051ark4
Contributor I

Hello,   I am hoping someone can tell me where I can find the actual  ICP algorithm for the P89LPC901.  I see there are some devices, like from Flash Magic, however.  I wish to design/build my own programmer.    I am interested in ICP programming at this point, NOT IAP.   Thank you.

0 Kudos
Reply

3,474 Views
grgsaliba
Contributor I

It seems to be obsolete as well.

Is there any documentation about the NXP ICP protocol ?

I'm not familiar with LPC microcontrollers but well experienced with other brands, I'm finding it strange that there seems to be no legacy ICP tool from NXP, was there any?

0 Kudos
Reply

3,472 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

George Saliba

I have an old backlog about ICP on my disk. see attached. Hope this will help you.

Have a nice day

Jun Zhang

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply

3,472 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

George,

I suggest you check if ic1000 is available for sale.

iSystem iC1000 PowerEmulator 

Besides, you can also consult:

Advin SpeedPro series
BPM various programmers
CooCox CoFlash
Data I/O various programmers
Elnec various programmers
ESAcademy FlashMagic ISP SW
FDI USB-ICP-LPC9xx
Hi-Lo Systems ALL-100
Leap Leaper / SU / AH
Phyton ChipProg series
pls UDE MemTool
Raisonance RFlasher7
SMH Technologies FlashRunner for LPC
Xeltek SuperPro series
ZLG SmartPRO / EasyPRO

Have a great day,
Jun Zhang

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply